Other Parts Discussed in Thread: TPS66021
We have a custom product we have developed that is using a USB-C connector to implement a SS port. The port is a DRP so additional circuitry has been added to support this feature aside from the HD3SS3220 switch. In my design I'm using 100nF AC coupling caps on TX1/TX2 and RX1/RX2 lines. However, I noticed some posts have suggested to use 220nF instead of the 100nF. I also noticed another forum post suggested using 330nF coupling caps on the RX lines. What is the correct values to utilize? How are those values determined? Could this be causing my issue?? Also I'd like to have someone review my schematic. Is there an email address I can send my schematic sheet too.