I'm trying to find the thermal resistance from the junction to the board (JB) and the case (JC) for the device TL16C752D. Is someone able to provide this information?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm trying to find the thermal resistance from the junction to the board (JB) and the case (JC) for the device TL16C752D. Is someone able to provide this information?
Tim,
I will get this information for you, however, it can take up to two weeks to obtain this information. Once this is obtained, I'll follow up here. I will be getting thermal data for the TL16C752DPFBR package.
Best,
Danny
Tim,
I hope things are well. The results you requested for TL16C752DPFBR are below:
Characteristic | Value [°C/W] |
Theta JA-High K | 63.5 |
Theta JC, top | 18.0 |
Theta JB | 27.3 |
Psi JT | 0.7 |
Psi JB | 27.1 |
Theta JC, bottom | N/A |
Best,
Danny