This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THVD1500: Competitor table between AZRS3082.RDG,SH65HVD3082EDR,THVD1500DR

Part Number: THVD1500
Other Parts Discussed in Thread: THVD1419, SN65HVD3082E

HI Sir

Could you help to share the Competitor table between AZRS3082.RDG,SH65HVD3082EDR,THVD1500DR

thanks

  • Hi,

    THVD1419 might be a better match for AZRS3082, since both have surge protection feature. Here is the comparison among all 4 devices.

    Device SN65HVD3082E THVD1500 ARZS3082 THVD1419
    Duplex Half Half Half Half
    Number of TX 1 1 1 1
    Number of RX 1 1 1 1
    Supply voltage(s) (Nom) (V) 5 5 5 3.3,
    5
    Signaling rate (Max) (Mbps) 0.2 0.5 0.115 0.25
    Fault protection Feature - Extended Fault protection NO NO NO NO
    Fault protection (V) -9 to 14 -18 to 18 -13 to 13 -15 to 15
    Integrated IEC ESD protection Feature - Integrated IEC ESD protection NO YES YES YES
    IEC 61000-4-2 Contact Discharge (+/- kV) Need external circuit 8 30 8
    IEC61000-4-2 Air-gap Discharge (+/- kV) Need external circuit 10 30 30
    Integrated IEC EFT (Noise Immunity) Feature - Integrated IEC EFT (Noise Immunity) NO YES YES YES
    IEC61000-4-4 EFT (+/- kV) Need external circuit 2 4 4
    Integrated IEC Surge Protection Feature - Integrated Surge protection NO NO YES YES
    IEC61000-4-5 Surge (+/- kV) Need external circuit Need external circuit 1.26 2.5
    Extended Common Mode Feature - Extended common mode NO NO NO YES
    Common mode range (V) -7 to 12 -7 to 12 -7 to 12 -12 to 12
    Number of nodes 256 256 256 256
    HBM ESD (kV) 15 16 15 16
    ICC (Max) (mA) 0.9 0.66 0.6 3
    Temperature Range (°C) -40 to 85 -40 to 125 -40 to 85 -40 to 125

    Regards,

    Hao