Hello,
How to define the block size? Take YUV422 8bit for example, the below post describes the block size is 2,
but according to the MIPI CSI-2 spec, the packet size is 4byte, isn't 4 block size?
In addition, the datasheet of DS90UB954 also describes the block size, I am confused about this, for example, an RGB888 pattern would consist of 3-byte pixels and therefore require a 3-byte block size. A 2x12-bit pixel image would also require 3-byte block size, while a 3x12-bit pixel image would require nine bytes (two pixels) to send an integer number of bytes. Could you please help to explain it how to define the block size?
Best regards
Kailyn