This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLIN2029-Q1: 24 V applications

Part Number: TLIN2029-Q1
Other Parts Discussed in Thread: TLIN1029-Q1

Hi team,

Thanks for your support.

I have two questions about TLIN1029-Q1 and TLIN2029-Q1.

Q1:TLIN2029-Q1 supports 24V applications and  TLIN1029-Q1 supports 12V applications. Is their difference only reflected in  wider operating voltage and additional bus-fault protection?

Q2:For TLIN 2029-Q1,if the 24V(VBAT) can be directly connected to the LIN transceiver? So the voltage of LIN bus is 24V?

Thanks,

Ivy