RS485 transreceiver with 330 ohm internal termination resistor

Prodigy 150 points

Replies: 1

Views: 24

Dear Sir,

There is particular requirement  for the RS485 transreceiver with a SW selectable line to line termination/bias for RS485 with 330-ohm termination and 680ohm pull-up to +3.3V & 680ohm pull-down to 0 V.

Is there any part you can suggest?

BR

SM

1 Reply