This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Original question:
DS250DF230: Use retimer to generate and check PRBS signals
Replies: 5
Views: 77
Part Number: DS250DF230
Hi:
I'm using DS250DF230 in the design, and I'm doing the PRBS test. The link under test is like this:
322.265625MHz -> CABLE -> Retimer (10.3125Gbps) -> oscilloscope
I want to use the retimer to generate PRBS. But after I configured the registers, there're no signal outputs. My configuration sequence is shown below:
Referenced from Programmer's guide(SNLU182D)
// Configuration0xFC, 0x01 , 0xFF 0xFF, 0x03 , 0x030x0A, 0x0C , 0x0C
0x60, 0x90 , 0xFF 0x61, 0xB3 , 0xFF 0x62, 0x90 , 0xFF 0x63, 0xB3 , 0xFF 0x64, 0xFF , 0xFF 0x09, 0x04 , 0x04 0x18, 0x10 , 0x70
0x1E, 0x00 , 0x100x0A, 0x00 , 0x0C
//PRBS gen0x2E, 0x04 , 0x04 0x30, 0x01 , 0x030x1E, 0x10 , 0x100x79, 0x00 , 0x200x79, 0x20 , 0x20 0x30, 0x00 , 0x080x30, 0x08 , 0x08 0xA5, 0x80 , 0xE0
Any advice will be appreciated, thanks!
Hi,
Can you confirm whether you are using CAL_CLK_IN = 25MHz on your board?
Cordially,
Rodrigo Natal
HSSC Applications Engineer
In reply to Rodrigo Natal:
Hi, Rodrigo
I have confirmed that I'm using CAL_CLK_IN = 25MHz(50ppm) on my board.
Regards,
In reply to user6207997:
What values are you observing for the channel registers below on the retimer channel in question that you are working to configure as PRBS generator?
I observed the below channel register values.
0x02 -> 0x00
0x27 -> 0x00
0x28 -> 0x00
0x78 -> 0x20
0x8F -> 0xEA
The retimer CDR does not appear to be locking to your 322.265625MHz reference signal. Some additional suggestions
Table. Set CTLE Boost Value
STEP
SHARED/ CHANNEL REGISTER SET
OPERATION
REGISTER ADDRESS [HEX]
REGISTER VALUE [HEX]
WRITE MASK [HEX]
COMMENT
1
Channel
Write
2D
08
Enable CTLE boost override
2
03
00
FF
Set CTLE boost to 0x00.