This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HD3SS3220: USB Type-C Functional Test Error

Intellectual 1075 points

Replies: 3

Views: 46

Part Number: HD3SS3220

Hi there, 

My customer is evaluating HD3SS3220 used for USB interface of his system. He is now doing the USB Type-C Functional Test, but error message occurred like this.

    1. TD 4.1.2 Unpowered CC Voltage Test

            The PUT's CC voltage is not in vOPEN range.

    2. TD 4.3.1 Sink Connect Source Test

            The PUT does not start USB communication.

    3. TD 4.3.4 Sink Connect Try.SNK DRP Test

            The PUT does not continue to provide Rd on the CC pin for the duration of this test.

I am wondering if 1st problem was due to HD3SS3220's dead battery mode(datasheet pp.19). It sets the Rd as 5.1kohm so 1st test could not pass.

If so, can this operation mode be switched off?

And 2nd & 3rd problem were due to HD3SS3220's debug accessory  mode(datasheet pp.23)? This mode is enabled by default, but the test requires debug accessory mode to be off. So the 2nd & 3rd test could not passed.

Is my consideration correct? Please let me know if there are any other possible causes.

Thank you and best regards,

Zeming

3 Replies

  • Hi Zeming,

    Do you have the test report that I can review? I would like to confirm your explanation for the failures. TD 4.1.2 failure is most likely fails due to dead battery mode. TD 4.3.1 implies that TVS did no see USB enumeration process which can happen if TVS does not present termination, switch is not in correct position or USB Host is not ready to communicate. TD 4.3.4 may be caused by accessory mode support but should double confirm. Is accessory support marked in the VIF?

    Best, 

    Malik

  • In reply to Malik Barton57:

    Hi Malik,

    I have emailed the test report to you. Please help check the error.

    Regards,

    Zeming

  • In reply to Zeming Kong:

    Hi Zeming,

    Understood we can move this to an internal thread. Closing this E2E thread. 

    Best, 

    Malik

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.