This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UR910-Q1: DS90UR910 output signal is abnormal even lock pin and pass pin are in high status

Part Number: DS90UR910-Q1
Other Parts Discussed in Thread: DS99R421, DS90UR124

Hi,

We use DS90UR910  as deserializer to convert FPD Link to mipi CSI, and we configure it in Gen 2 mode, but nothing output now, the output signal is abnormal.

The input signal comes from car main unit, which can display on the car monitor without any problem. On the hardware level, lock pin and pass pin work fine, both of them are in high status, so what other things should we configure to make the output signal become normal, maybe some register value need to adjust? Hope to get some help. Thanks

Here is the output signal showed on the oscilloscope.