Replies: 14
Views: 169
Part Number: TPS65987D
Tool/software: TI C/C++ Compiler
I want to supply 100W using TPS65987D.
I tried to supply using TPS65987 EVM, but it was negotiated at 20V3A.
I want to confirm setting Is there a way to set "Type C Current" to 5A?
"Type C Current" on GUI was only Defolt,1.5A, 3A.
Best Regard
Kudo
Hello,
Do you mean that you configured PD controller for 5A PDO but its making 3A contract only? if yes, please check if the cable is capable of supporting 5A (you can find out the cable capability from the datasheet of the cable or PD trace).
Thanks
Prajith
In reply to Prajith Cheerakkoda:
Hello Prajith san
Thank you replay
I was using the following cablewww.mco.co.jp/.../UPD-220 / BKThe package said it was compatible with 20V / 5A / 100WCan this Cable use ?
I will list the confirmed PC.www2.razer.com/.../razer-blade-stealthrazer blade stealth 13When I connected it from the AC adapter, it was 20V 4.2A.But from TPS65987EVM ,it was 20V2.7A.
TPS65987EVMPP1 20V (external power supply)PP2 5A (DCDC_VAR)
SWS1, S2 Defolt
Could you please confirm the setting?Also, do I need to change the TPS65987EVM in terms of hardware?
In reply to user5034648:
I attached Config setting
Would you confirm this data?
Hi Kudo-San,
Please share the pjt file that you are using.
Hallo Prajith san
I try to upload pjt file .
Would you confirm it ?
If you can't confirm ,please teach me how to attach this prj file .
Shuji.kudo
tps65987d.pjt
Hi Kudo-san,
As I see" source PDO3 negotiated " in GPIO 20 event, but only two source PDOs is selected.
Is the setting right with your hardware circuit?
In reply to Bing Hwang:
HelloI used PC is 100W compatible .I don't use other PC.So I Prepared only 5V and 20V .
20V to PP15V to PP2
By TPS65987EVM,I connected PP1 = SYS_VCC(20V) and PP2 =DCDC_VALIs there a way to supply 20V 5A with this specification?
Would you possible to send a bin file or pjt file that can confirm 20V5A using TPS6587EVM?
Would you tell me if we need to change hardware settinng by TPS65987EVM ?
TPS65987DDH_20V_5A.pjt
Kudo-san,
You can try the latest .pjt file I attach, I have verified the .pjt and it can communicate 20V @5A successfully.
I want to explain two points of this case.
1. Since you use external power to power up 20V @5A, you don't need to set GPIO 20 event at PDO3. After the communication of PD, the 20V source path you map will be enabled automatically;
2. The failure of 5A communication is caused by e-mark not powered. You used standard configuration template, which doesn't contain Vconn related configuration, so the e-mark was not powered, so the cable didn't tell PD controller its current capability @5A, and ultimately cause the 5A communication failure.
In addition, I want to point out that your setting of GPIO20 @PDO3 will lead to error if you want use DCDC to generate 20V PDO.
---------------> You only configured two PDOs in "Transmit Source Capabilities" register, so the PDO with 20V @5A is PDO1 rather than PDO3; only if you configure four PDOs, you will use PDO3. And on TPS65987D EVM, the voltage level is determined by GPIO which will control the DCDC converter to send out the relative voltage level. We use GPIO14/ GPIO15/ GPIO17/ GPIO20 to generate 5V/ 9V/ 15V/ 20V. And actually 5V is generated naturally by DCDC output, GPIO14 is only used to light up the 5V indicator LED.
In conclusion, the configuration you set makes no sense in this case because you use external power source (SYS_PWR) to generate 20V on VBUS. But if you want to use DCDC to generate 20V on VBUS, you need to set "source PDO1" on GPIO 20 rather than "source PDO3" because you just have set two PDOs to transmit source capability.
Hi Bing Hwang ,
I check the Last Post , It say recommended to attach 5V to the PP_Cable pin. For VCONN provide power to e-marked Type-C cables.
Now I use Source Board is TIDA-050012, It seems connect PP_Cable pin to Ground,
If want to use e-mark need re-work on TIDA-050012 connect PP_Cable pin attach 5V?