Hi all
Would you mind if we ask DP83825I?
On the our customer's board, voltage swing(PMD out) with 100Base-TX) is more than ±1.05V.
(Please refer to the following figure. CH1=TD_P pin, CH2=TD_M pin)
<Question1>
How much is the maxmium and minimum value of PMD out in case of 100Base-TX?
We quess that it will be within Min=±0.95V and Max=±1.05V.
Is it correct.
<Question2>
If the value is from Min=±0.95V to Max=±1.05V, the device might have some troble.
Should we check Rbias pin?
And then, how much is the voltage of Rbias?
And this voltage is static DC level?
Kind regards,
Hirotaka Matsumoto