Hi,
I wanted to use this re-driver with intel platform.
From the platform requirement on the USB3.2 re-driver, it stated :
It is recommended that OEMs use active mux/retimer/redriver parts from 3rd party vendors which meet below requirements to avoid Electrical Over Stress (EOS) on USB 3.2 receiver lines: During power on and receive detect phase, recommended transmitter common mode voltage (Vcm) and impedance values:
(i) If (Vcm <= 1.2V), Repeater Impedance >= 1K ohm ELSE;
(ii) (Vcm+Rx.detect pulse amplitude <= 2.2V) AND (Repeater Impedance >= 4.5K ohm).
Is the TUSB1002a comply with these requirements?
Thank you.
-Desmond