Replies: 3
Views: 46
Part Number: TPS65988
I need to make the voltage output of PDO1 5.25V, how do I need to operate it?
I use TPS65988 and TPS55288 to connect with I2C1. The PDO1 setting of TPS65988 is 5V/3A, but I need PDO1 to actually output 5.25V. What should I do?
Hello,
To comply with the USB PD specification, the PD controller must provide the fixed 5V/3A by default, if it is configured as a source. However, since you would like to source 5.25V/3A, you can simply add in another PDO and use this Source PDO2 to provide the 5.25V.
Thank you,
Hari
In reply to Hari Patel1:
Hi Hari,
Thanks for your reply,
but I want to know if there is a way to make PDO1 display 5V, but actually output 5.25V.
thank you
In reply to user6461981:
Unfortunately, no you cannot output more than the advertised voltage for normal operation.