Hi,
We are using SN65HVD10DR RS 485 IC in all product. In one product (mPod-L) it is used as Master & in Energy Meters as a slave.
We had tested 32 slaves (Energy Meter) with RS485 converter. It works fine without any terminating resistor R110 (DNP). The cable length is <10mtrs.
But during testing with mPod-L as a Master, after connecting Fail safe resistor (R104,R112) it started working with 32 slave devices. Before that it works up to 4 slaves.
Does Fail safe resistors are require if it is used as Master ?
Please refer below schematic FYR.
Appreciate prompt response.
Thanks,
Dattatray