Other Parts Discussed in Thread: TS3USB221E, TUSB216, TUSB1064
Hello TI team
The MacPro typec receptacle USB2.0 can only work A6 A7 or B6 B7 that mean when the device directly insert receptor the A6 A7 PIN work USB 2.0 ,and flipping insert receptor B6 B7 PIN work USB 2.0, so use the TUSB2E22 can cross the USB 2.0 signal . But the TUSB2E22 is eUSB to USB, Now I am looking for cross signal device USB 2.0 to USB 2.0 , will you can recommend some part number.
below is the system diagram .