Hi team,
My customer have several questions about TUSB4041I. Need your kind answers, thank you very much.
- Is there any requirement for Test-pin pull-down resistance value and its accuracy?
2. In customer's application, TUSB4041I is used for internal USB extension, not for external USB, so customer don't use USB charging function. Can they just float PWRCTL pin? And also float OVERCUR pin?
3. What's the EEPROM used for? If customer don't add EEPROM, what's the impacts, do they have to add?
4. Is it OK to set FULLPWRMGMTz/SMBA1 = 1, GANGED/SMBA2/HS_UP = 1 in customer's application?
5. Could you please explain the Automatic mode? If customer disable this mode, what's the impacts, will it affect the device normal operation?
Thank you!