This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9557: PCA9557 can not be reset

Part Number: PCA9557

Hi Team

  My customer Zhuzhou is using PCA9557 and met some problem for reset function.

  I've read the previous discussion for PCA9557 and there're 3 ways to reset the device:

1. keep VCC low longer than 100ms and Power on less than 10ms, I've tried many time and failed to reset the device;

2. Reset pin keep low longer than 400ns, still failed;

3. 9 clock pulses, succeed, but I don't know why it worked, any explanation or potential risk by using this way?

  And it seems we don't have TCA9557 to replace PCA part, any recommendations?