Other Parts Discussed in Thread: TPD3S714-Q1
Hello Sirs,
Is there solution could provide GPIO Short-to-Battery & Short-to-ground protection.
This is for Automotive proprietary connector interface .
Many thanks !
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Sirs,
Is there solution could provide GPIO Short-to-Battery & Short-to-ground protection.
This is for Automotive proprietary connector interface .
Many thanks !
Hi Terry,
Thanks for reaching out. For Short-to-Battery and Short-to-ground protection, please take a look at the TPD3S714-Q1. However, the TPD3S714-Q1 was designed primarily for the USB 2.0 interface so the device supports voltages from 0 to 0.3+Vin and has a Ron -3dB bandwidth of 860MHz. As long as these are compatible with your GPIO interface, it should be a suitable solution.