Part Number: TPS65983
Hi,there
When I verify the type c PD controller TPS65983 source function, I found that the PP_EXT to VBUS positive voltage transitions slew rate is out of the specification on datasheet, and I don't know how to meet the spec according the datasheet, is there any method to change the slew rate for positive voltage transitions?
Below is the source function test record, slew rate=66666V/S
and spec on the datasheet, slew rate=30000V/S Max
Thanks,
Picher