This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS4: SN65LVDS4

Part Number: SN65LVDS4

Need the absolute maximum junction temperature for the SN65LVDS4

  • Hello David,

    The Abs Max Junction Temperature is 140C. Please note that the Abs Max standard disclaimer applies here:
    "These are stress ratings only, and functional operation of the device at these or any other conditions beyond those indicated under Recommended Operating Conditions is not implied. Exposure to absolute-maximum-rated conditions for extended periods may affect device reliability".

    Regards,
    Yaser