This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN330: multiple TCAN330 connection

Part Number: TCAN330

Hi,

I have a question when using TCAN330. When I use multiple TCAN330, their CANH and CANL connect respectively, as the attachment picture. My question is, when part2 and part  are  not powered or there is large leakage at CANH/CANL prorts of  part2 or part3,maybe both of them, but part1 is powered with 3.3V, what does this impact part1's wave form of CANH/CANL? 

Thans for your apply.