Dear DP83894C experts,
The spec says the following about the MII RX_ER
"MII RECEIVE ERROR: Asserted high synchronously to RX_CLK to
indicate that an invalid symbol has been detected within a received
packet in 100 Mb/s mode."
It does not elaborate on the role of that signal in 10 Mbits/s mode.
1) Does that imply that is has no role in 10 Mbits/s mode ?
2) Is the default value of that signal high, and is only set to 0 upon a no RX_ER detection ? If so won't it interfere with teh 10 Mbits/s mode ?
Kind regards,
Rocco