This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN330: Internal pull-down(s)

Part Number: TCAN330

Hi,

do you have a approximately value of the internal pull-down(s) of SHDN and S (for TCAN330DCN) ?

Thx in advance !

BR

  • User,

    For both pins, the high-level leakage current can be used to find the approximate pull-down value. Since internally these are pulled to ground, and the high-level leakage current is measured with 3.6V applied to the pin, Ohm's law can be used to find out the resistance value. 3.6V / 10uA = 360kΩ

    Please let me know if you have any other questions.

    Regards,