This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848I: No link, stuck during Auto-MDIX

Part Number: DP83848I


Hi,

I'm having trouble with the DP83848I to establish a link.

  • The communication partner is one factor. I tried different Network Interface Cards and switches: the success of establishing a valid link varies between 5% and 100%.

  • The success rate between specific devices from one production batch also varies strongly.

So I took a closer look at the status registers:

  • BMSR: Basic Mode Status Register

  • PHYSTS: PHY Status Register

  • ANLPAR: Auto-Negotiation Link Partner Ability Register

  • ANER: Auto-Negotiate Expansion Register

What I found out so far:

  • After plugging in an Ethernet cable, nothing happens with regard to the status registers:

    BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 / ANER:0x0004$

    BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 / ANER:0x0004$

    BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 / ANER:0x0004$

    BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 / ANER:0x0004$

  • When I pull the plug, the Auto-MDIX functions starts swapping the MDI pairs (PHYSTS:0x4000 means "MDI pairs swapped"):

    BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 / ANER:0x0004$

    BMSR:0x7849 / PHYSTS:0x4000 / ANLPAR:0x0000 / ANER:0x0004$

    BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 / ANER:0x0004$

    BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 / ANER:0x0004$

    BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 / ANER:0x0004$

    BMSR:0x7849 / PHYSTS:0x4000 / ANLPAR:0x0000 / ANER:0x0004$

    BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 / ANER:0x0004$

    BMSR:0x7849 / PHYSTS:0x4000 / ANLPAR:0x0000 / ANER:0x0004$

  • Now if I put in the plug again, the MDI swapping stopps again. If the MDI-swapping was in the "right" state I'm lucky and I get link. If not, removing and inserting the plug will eventually result in a link.

I double checked the schematics and the PCB layout but can't find any mistakes. Any ideas what could cause this behavior?

Regards,

Florian

  • Hi Florian,

    Are you changing any registers on the PHY via software or straps? Have you checked the link with another DP83848?

    -Regards

    Aniruddha

  • Hi Aniruddha,

    thanks for you reply, All of the strapping pins have external pullups or pulldowns. Their setting - pullup or pulldown - corresponds to the default strapping (internal pullups/pulldowns) from the datasheet.

    The registers are also changed via software to their defaults after every power cycle. Maybe this is a little bit to much of redundancy. But it shouldn't do any harm it think.

    I can reproduce this error with others of our interface electronics containing the DP83848. Or did you mean I should connect two DP83848 together? Well, I did this anyway. The result is: sometimes a 100 Mbit Full-Duplex link is established like it should. But sometimes only a Half-Duplex link can be established. I looked at the registers but didn't really understand what happens. Maybe you have any ideas.

    Registers after power up:

    PHY registers:
    BMCR: 0x3100
    BMSR: 0x7849
    ANAR: 0x01E1
    ANLPAR: 0x0000
    ANER: 0x0004
    ANNPTR: 0x2001
    PHYSTS: 0x0000
    MICR: 0x0000
    MISR: 0x0000
    FCSCR: 0x0000
    RECR: 0x0000
    PCSR: 0x0100
    RBR: 0x0021
    LEDCR: 0x0000
    PHYCR: 0x8021
    10BTSCR: 0x0904
    CDCTRL1: 0x0000
    EDCR: 0x6011
    AUTO-NEGOTIATION: BMCR: 0x1000 / ANAR:0x01E1

    Connecting two DP83848 together, success, 100 Mbit Full-Duplex:

    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x4000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x4000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x4000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x4000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x4000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x4000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x4000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x4100 / ANLPAR:0x41E1 // PHYCR:0x8021 $
    >BMSR:0x7869 / PHYSTS:0x4115 / ANLPAR:0x41E1 // PHYCR:0x8021 $
    #-X-#: AN Done, Result=3 / 27
    >successful<
    100 Mbps, Full Duplex

    Connecting two DP83848 together, failure, 100 Mbit Half-Duplex:

    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0000 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0100 / ANLPAR:0x41E1 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0900 / ANLPAR:0x0000 // PHYCR:0x8021 $  => False Carrier event has occurred since last read of FCSCR??
    >BMSR:0x7849 / PHYSTS:0x0900 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0900 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0900 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0900 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0900 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0900 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0900 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0900 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0900 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x4900 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x0900 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x4900 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x4D00 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x4D00 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7849 / PHYSTS:0x4D00 / ANLPAR:0x0000 // PHYCR:0x8021 $
    >BMSR:0x7869 / PHYSTS:0x4D11 / ANLPAR:0x0081 // PHYCR:0x8021 $
    #-X-#: AN Done, Result=3 / 25
    >Not supported by Link Partner<
    Settings used: Examined Speed / Half Duplex (default)
    100 Mbps, Half Duplex

    Regards,

    Florian

  • Hi Florian,

    Can you share the schematics of the board? The power up register settings of the PHY seem ok.

    -Regards

    Aniruddha

  • Hi Aniruddha,

    can I send you the schematics via private message?

    Regards,

    Florian

  • Hi Florian,

    Yes, private message on E2E is should be fine. We also have a app note to check the schematics for DP83848: 

    You can also in parallel check the schematics while I am reviewing it.

    -Regards

    Aniruddha

  • Hi Aniruddha,

    sorry for spamming the forum. But I think you have to accept my friendship request before I can send you a private message.

    Meanwhile I'll work through the app note.

    Regards,

    Florian

  • Hi Florian,

    Apologies for the delay, there was some mix-up in thread tracking and this thread got dropped off from my list of active questions. I have accepted your connect request on E2E so you should be able to send confidential material over to me via private chat. I also have your schematics and have some questions about it.

    Is RBIAS resistor 1% tolerance?

    Are the 49.9 ohm resistors 1% tolerance?

    Does the 50MHz clock meet the datasheet requirement?

    Does the magnetics meet the datasheet requirement?

    Do you perform a hardware reset or power cycle after every link up test?

    How long do you wait before you consider link attempt a failure and move to the next iteration?

    -Regards

    Aniruddha

  • Hi Aniruddha,

    to answer your questions:

    • The resistor tolerances are 1%.
    • Regarding the 50Mhz clock: it seems that the jitter requirements aren't met. I'm going to test with an oscillator with tighter jitter specs and report back.
    • We use one of the recommended magnetics from the app note (J0011D21BNL).
    • I did the link up test in different ways:
      • power cycles between consecutive tests
      • just disconnecting and reconnecting the ethernet cable
      • initiating a software reset via Masic Mode Control Register
      • The success rate of getting a link is independent from the approach it take.
    • I consider the link attemp a failiure after a couple of seconds. In my excperience if it works it takes about 2 s at max. If it doesn't, waiting for even minutes won't result in a link.

    Best regards
    Florian

  • Hi Florian,

    Thanks for the update. Let me know if improving the clock helps improve the link up. For your link up time, can you also try relaxing your cut-off time to 6-8 seconds when you re-test. There is no max link up defined in the IEEE standard and sometimes normal link up can take 5+ seconds. 

    -Regards

    Aniruddha

  • Hi again,

    it took me some time to do a test with a different clock. I disconnected the previously used clock (from the FPGA) and used the optional dedicated 50 MHz oscillator on the PCB (also ensured it meets the requirements from the datasheet). It didn't make any difference.

    I noticed that it can take pretty long for the link to establish. Sometimes like 20 seconds. But in most cases if the link isn't established within an few seconds it never will.

    I still think it has something to do with the AUTO-MDIX feature. The state machine in the PHY stops swapping the pairs when the cable is plugged in:

    • Either the PHY 'thinks' the pair's polarity is ok, so no reason to swap them...
    • or the state machine get's stuck in a certain state. Are there any registers which could provide insight?


    I'm going to measure MDI-signals before and after the magnetics again. Maybe I can find out something that way.

    Best Regards,
    Florian

  • Hi Florian,

    There are no registers that will till the current status of the Auto-MDIX routine but register 0x10[14] should tell you if the pair are normal or they are swapped. Another experiment that you can try to isolate the problem is to force the PHY in either MDI or MDIX and see if that helps resolve your issue. You can force MDI/MDIC via register 0x19[15:14].

    -Regards

    Aniruddha

  • Hi Aniruddha,

    thanks for not giving up on me :-)

    Forcing MDI/MDIX via register actually works. It might be a viable workaround.

    But I'm still wondering where this whole behaviour comes from. It might be an indication that something is fundamentally wrong which might lead to further problems in the long term.

    Regards,

    Florian

  • Hi,

    I think I got to root of the problem. And it's very likely that it isn't the DP83848I.
    I had a closer look at the Fast Link Pulses (FLP) during Auto-Negotiation:

    • The test PC that I used for all my tests was particulary "good" reproducing the link problem.
    • As it turns out, the FLPs that the DP83848I receives from the test PC on it's RX-pair are significantly smaller than compared to those the TX-Pairs (see the picture)
    • I double checked this by measuring the test PC signals without any link partner physically connected to it.
    • Then I used a longer 10 m Ethernet cable for the connection betwenn my DUT and the test PC. As expected this attenuated the FLPs by another few milivolts.
    • What was utterly unexpected: the link problem was gone!

    My guess what happend:

    • The low amplitude FLPs were above the threshold of the DP83848I to detect them (at least partially). Though it did not switch to MDIX
    • The low amplitude may have caused receive errors that prevented to establish a proper link
    • With the longer cable the FLPs are below the threshold of the DP83848I. Though it only sees FLPs on the TX-pairs, switches to MDIX and everything works fine.

    I'm going to look for other PCs or Ethernet switches where the link problem was observed. I will get back an report if I found out anything new.