This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS4: LVSD driver 1.8V

Part Number: SN65LVDS4
Other Parts Discussed in Thread: SN65LVDS179, SN65LVDS1

Hi sir,

We are desperately looking for 1.8V supply LVDS drivers and receivers (Our device is 1.8V). We found a LVDS receiver from TI (TI SN65LVDS4) that could operates from a 1.8V or 2.5V core supply, but could not find a corresponding LVDS driver.
Therefore, we have the following questions:

1. Do you know any 1.8V supply LVDS driver available in the market?
2. If not, can I use 2.5V or 3.3V supply LVDS drivers (such as TI SN65LVDS1 or TI SN65LVDS179) under 1.8V voltage supply?
I noticed that the maximum supply voltage range for these chips is usually from -0.5 to 4V. Are these chips functional well under 1.8V supply?

our device only accepts 1.8V LVDS input signals. So we also need a 1.8V LVDS driver. Do you have any ideal how to do that?
If I use 2.5V or 3.3V LVDS driver under 1.8V voltage supply. Is that Ok to do that?

Thanks a lot in advance.

Regards,

M