Please note that E2E has undergone a major upgrade. Before logging in, please clear ALL your browser's cache and cookies.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD82: SN65HVD82 working voltage

Part Number: SN65HVD82
Other Parts Discussed in Thread: THVD1410, SN74LVC1G34

Hi Team,
I've some doubts about designing a circuit using SN65HVD82.
In the datasheet, it is clearly mentioned that the VCC is 4.5V to 5.5V. Do I need a level shifter at its pins like R, D, and DE&~RE pins since my controller is working in 3.3V logic or can I connect the VCC of the SN65HVD82 to 3.3V?.