Other Parts Discussed in Thread: SIGCONARCHITECT, USB2ANY
Dear e2e members,
I'm currently trying to export a DS125DF1610 configuration to an EEPROM hex file that is written to an AT24C16C EEPROM where the retimer shall get its configuration from in normal operation.
For debugging purposes, I have the option of connecting to this retimer with USB2ANY/SigConArchitect.
I used the following settings for exporting the EEPROM:
Common Channel? --> NO
Address Map Enabled --> NO
EEPROM >256? --> YES
Enable CRC --> NO
No. of Device: 1
EEPROM Size: 2048 Bytes
Device Adress: 0x30
So I pretty much went with the default configuration of the retimer (see config file below), saved it as *.cfg file and then went on to the EEEPROM page, exporting the
settings as *.hex file. I wrote the settings to the EEPROM, power-cycled the device and surprise - the settings don't work anymore. I can exclude a read/write error, since the settings in the hex file are being parsed
correctly to the retimer, it rather seems that something during conversion process to .*hex file went wrong.
For example, lets take the setting stored in SMBUS-Register 0x13 (for channel 0A), according to my .cfg file, they shall be value(SMBUS_0x13)=0x90.
The relevant parts of this SMBUS register are stored in EEPROM address byte 0x08, according to TI document "Understanding EEPROM programming for 10G to 12.5G retimers".
So in my case I get value(EEPROM_HEX_0x08)=0x10 after generating the hex file. According to my understanding, the EEPROM header bytes shall not be counted here.
If I take the register map of above mentioned document, the value(EEPROM_HEX_0x08)=0x10 means that
value(SMBUS_0x13) is set to 0x88 after loading the EEPROM contents! Which is exactly what I read from this SMBUS register after loading the EEPROM. Which is not what I
originally configured.
This register is just an example of many others that are not applied correctly.
So my questions are:
- Are there any known bugs to the EEPROM hex file generator in SigConArchitect?
- Is there any other EEPROM generation tools/scripts/spreadsheets that you could possibly provide? I'm currently pretty sure that I have to generate the EEPROM contents by hand, so any helping tools are welcome....
Generated EEPROM hex (First bold part is the header, second bold part the hex value mentioned above:
:200000002000100000002804D00018100100004000E47900002607F20436411887E7F000DE
:2000200001AA1E3800082082000014001861820A860304844415023294658642BAEB4BAEFF
:20004000ACCCB5280000000001A2240000003211A1204FA04E00000861F9F80000002804BD
:20006000D00018100100004000E47900002607F20436411887E7F00001AA1E38000820822F
:20008000000014001861820A860304844415023294658642BAEB4BAEACCCB52800000000F5
:2000A00001A2240000003211A1204FA04E00000861F9F80000002804D00018100100004079
:2000C00000E47900002607F20436411887E7F00001AA1E3800082082000014001861820AEF
:2000E000860304844415023294658642BAEB4BAEACCCB5280000000001A2240000003211A4
:20010000A1204FA04E00000861F9F80000002804D00018100100004000E47900002607F2A6
:200120000436411887E7F00001AA1E3800082082000014001861820A86030484441502326C
:2001400094658642BAEB4BAEACCCB5280000000001A2240000003211A1204FA04E000008DB
:2001600061F9F80000002804D00018100100004000E47900002607F20436411887E7F0005B
:2001800001AA1E3800082082000014001861820A860304844415023294658642BAEB4BAE9E
:2001A000ACCCB5280000000001A2240000003211A1204FA04E00000861F9F800000028045C
:2001C000D00018100100004000E47900002607F20436411887E7F00001AA1E3800082082CE
:2001E000000014001861820A860304844415023294658642BAEB4BAEACCCB5280000000094
:2002000001A2240000003211A1204FA04E00000861F9F80000002804D00018100100004017
:2002200000E47900002607F20436411887E7F00001AA1E3800082082000014001861820A8D
:20024000860304844415023294658642BAEB4BAEACCCB5280000000001A224000000321142
:20026000A1204FA04E00000861F9F80000002804D00018100100004000E47900002607F245
:200280000436411887E7F00001AA1E3800082082000014001861820A86030484441502320B
:2002A00094658642BAEB4BAEACCCB5280000000001A2240000003211A1204FA04E0000087A
:2002C00061F9F80000002804D00018100100004000E47900002607F20436411887E7F000FA
:2002E00001AA1E3800082082000014001861820A860304844415023294658642BAEB4BAE3D
:20030000ACCCB5280000000001A2240000003211A1204FA04E00000861F9F80000002804FA
:20032000D00018100100004000E47900002607F20436411887E7F00001AA1E38000820826C
:20034000000014001861820A860304844415023294658642BAEB4BAEACCCB5280000000032
:2003600001A2240000003211A1204FA04E00000861F9F80000002804D000181001000040B6
:2003800000E47900002607F20436411887E7F00001AA1E3800082082000014001861820A2C
:2003A000860304844415023294658642BAEB4BAEACCCB5280000000001A2240000003211E1
:2003C000A1204FA04E00000861F9F80000002804D00018100100004000E47900002607F2E4
:2003E0000436411887E7F00001AA1E3800082082000014001861820A8603048444150000DE
:00000001FF
Config File:
0x0 Shared Registers_0x00 00
0x1 Shared Registers_0x01 71
0x2 Shared Registers_0x02 00
0x3 Shared Registers_0x03 00
0x4 Shared Registers_0x04 01
0x5 Shared Registers_0x05 08
0x6 Shared Registers_0x06 00
0x7 Shared Registers_0x07 05
0x8 Shared Registers_0x08 00
0x9 Shared Registers_0x09 00
0xA Shared Registers_0x0A 01
0xB Shared Registers_0x0B 40
0xC Shared Registers_0x0C 00
0xD Shared Registers_0x0D C6
0xE Shared Registers_0x0E 00
0xF Shared Registers_0x0F FF
0x10 Shared Registers_0x10 FF
0x11 Shared Registers_0x11 7F
0xFC Global Registers_0xFC 01
0xFD Global Registers_0xFD 00
0xFE Global Registers_0xFE 03
0xFF Global Registers_0xFF 00
0x0 Rx/Tx 0A_0x00 00
0x1 Rx/Tx 0A_0x01 80
0x2 Rx/Tx 0A_0x02 DC
0x3 Rx/Tx 0A_0x03 00
0x4 Rx/Tx 0A_0x04 01
0x5 Rx/Tx 0A_0x05 01
0x6 Rx/Tx 0A_0x06 01
0x7 Rx/Tx 0A_0x07 01
0x8 Rx/Tx 0A_0x08 60
0x9 Rx/Tx 0A_0x09 00
0xA Rx/Tx 0A_0x0A 50
0xB Rx/Tx 0A_0x0B 6F
0xC Rx/Tx 0A_0x0C 08
0xD Rx/Tx 0A_0x0D B4
0xE Rx/Tx 0A_0x0E 93
0xF Rx/Tx 0A_0x0F 69
0x10 Rx/Tx 0A_0x10 3A
0x11 Rx/Tx 0A_0x11 20
0x12 Rx/Tx 0A_0x12 E0
0x13 Rx/Tx 0A_0x13 90
0x14 Rx/Tx 0A_0x14 00
0x15 Rx/Tx 0A_0x15 12
0x16 Rx/Tx 0A_0x16 7A
0x17 Rx/Tx 0A_0x17 36
0x18 Rx/Tx 0A_0x18 40
0x19 Rx/Tx 0A_0x19 20
0x1A Rx/Tx 0A_0x1A A0
0x1B Rx/Tx 0A_0x1B 03
0x1C Rx/Tx 0A_0x1C 90
0x1D Rx/Tx 0A_0x1D 00
0x1E Rx/Tx 0A_0x1E E9
0x1F Rx/Tx 0A_0x1F 55
0x20 Rx/Tx 0A_0x20 00
0x21 Rx/Tx 0A_0x21 00
0x22 Rx/Tx 0A_0x22 00
0x23 Rx/Tx 0A_0x23 40
0x24 Rx/Tx 0A_0x24 00
0x25 Rx/Tx 0A_0x25 00
0x26 Rx/Tx 0A_0x26 00
0x27 Rx/Tx 0A_0x27 22
0x28 Rx/Tx 0A_0x28 36
0x29 Rx/Tx 0A_0x29 00
0x2A Rx/Tx 0A_0x2A 30
0x2B Rx/Tx 0A_0x2B 0F
0x2C Rx/Tx 0A_0x2C F2
0x2D Rx/Tx 0A_0x2D 04
0x2E Rx/Tx 0A_0x2E 00
0x2F Rx/Tx 0A_0x2F 36
0x30 Rx/Tx 0A_0x30 00
0x31 Rx/Tx 0A_0x31 20
0x32 Rx/Tx 0A_0x32 11
0x33 Rx/Tx 0A_0x33 88
0x34 Rx/Tx 0A_0x34 BF
0x35 Rx/Tx 0A_0x35 1F
0x36 Rx/Tx 0A_0x36 30
0x37 Rx/Tx 0A_0x37 00
0x38 Rx/Tx 0A_0x38 00
0x39 Rx/Tx 0A_0x39 00
0x3A Rx/Tx 0A_0x3A 00
0x3B Rx/Tx 0A_0x3B 3E
0x3C Rx/Tx 0A_0x3C 7D
0x3D Rx/Tx 0A_0x3D 35
0x3E Rx/Tx 0A_0x3E 43
0x3F Rx/Tx 0A_0x3F C7
0x40 Rx/Tx 0A_0x40 00
0x41 Rx/Tx 0A_0x41 01
0x42 Rx/Tx 0A_0x42 04
0x43 Rx/Tx 0A_0x43 10
0x44 Rx/Tx 0A_0x44 40
0x45 Rx/Tx 0A_0x45 08
0x46 Rx/Tx 0A_0x46 02
0x47 Rx/Tx 0A_0x47 80
0x48 Rx/Tx 0A_0x48 03
0x49 Rx/Tx 0A_0x49 0C
0x4A Rx/Tx 0A_0x4A 30
0x4B Rx/Tx 0A_0x4B 41
0x4C Rx/Tx 0A_0x4C 50
0x4D Rx/Tx 0A_0x4D C0
0x4E Rx/Tx 0A_0x4E 60
0x4F Rx/Tx 0A_0x4F 90
0x50 Rx/Tx 0A_0x50 88
0x51 Rx/Tx 0A_0x51 82
0x52 Rx/Tx 0A_0x52 A0
0x53 Rx/Tx 0A_0x53 46
0x54 Rx/Tx 0A_0x54 52
0x55 Rx/Tx 0A_0x55 8C
0x56 Rx/Tx 0A_0x56 B0
0x57 Rx/Tx 0A_0x57 C8
0x58 Rx/Tx 0A_0x58 57
0x59 Rx/Tx 0A_0x59 5D
0x5A Rx/Tx 0A_0x5A 69
0x5B Rx/Tx 0A_0x5B 75
0x5C Rx/Tx 0A_0x5C D5
0x5D Rx/Tx 0A_0x5D 99
0x5E Rx/Tx 0A_0x5E 96
0x5F Rx/Tx 0A_0x5F A5
0x60 Rx/Tx 0A_0x60 00
0x61 Rx/Tx 0A_0x61 00
0x62 Rx/Tx 0A_0x62 00
0x63 Rx/Tx 0A_0x63 00
0x64 Rx/Tx 0A_0x64 00
0x65 Rx/Tx 0A_0x65 00
0x66 Rx/Tx 0A_0x66 00
0x67 Rx/Tx 0A_0x67 20
0x68 Rx/Tx 0A_0x68 00
0x69 Rx/Tx 0A_0x69 0A
0x6A Rx/Tx 0A_0x6A 22
0x6B Rx/Tx 0A_0x6B 40
0x6C Rx/Tx 0A_0x6C 00
0x6D Rx/Tx 0A_0x6D 00
0x6E Rx/Tx 0A_0x6E 00
0x6F Rx/Tx 0A_0x6F 00
0x70 Rx/Tx 0A_0x70 03
0x71 Rx/Tx 0A_0x71 20
0x72 Rx/Tx 0A_0x72 00
0x73 Rx/Tx 0A_0x73 00
0x74 Rx/Tx 0A_0x74 00
0x75 Rx/Tx 0A_0x75 00
0x76 Rx/Tx 0A_0x76 22
0x77 Rx/Tx 0A_0x77 1A
0x78 Rx/Tx 0A_0x78 30
0x79 Rx/Tx 0A_0x79 10
0x7A Rx/Tx 0A_0x7A 00
0x7B Rx/Tx 0A_0x7B 00
0x7C Rx/Tx 0A_0x7C 00
0x7D Rx/Tx 0A_0x7D 48
0x7E Rx/Tx 0A_0x7E 13
0x7F Rx/Tx 0A_0x7F 3A
0x80 Rx/Tx 0A_0x80 04
0x81 Rx/Tx 0A_0x81 E4
0x82 Rx/Tx 0A_0x82 00
0x83 Rx/Tx 0A_0x83 00
0x84 Rx/Tx 0A_0x84 01
0x85 Rx/Tx 0A_0x85 00
0x86 Rx/Tx 0A_0x86 00
0x87 Rx/Tx 0A_0x87 00
0x88 Rx/Tx 0A_0x88 00
0x89 Rx/Tx 0A_0x89 02
0x8A Rx/Tx 0A_0x8A 89
0x8B Rx/Tx 0A_0x8B 00
0x8C Rx/Tx 0A_0x8C 00
0x8D Rx/Tx 0A_0x8D 02
0x8E Rx/Tx 0A_0x8E 1C
0x8F Rx/Tx 0A_0x8F 00
0x90 Rx/Tx 0A_0x90 00
0x91 Rx/Tx 0A_0x91 00
0x92 Rx/Tx 0A_0x92 00
0x93 Rx/Tx 0A_0x93 00
0x94 Rx/Tx 0A_0x94 00
0x95 Rx/Tx 0A_0x95 00
0x96 Rx/Tx 0A_0x96 04
0x97 Rx/Tx 0A_0x97 00
0x98 Rx/Tx 0A_0x98 0C
0x99 Rx/Tx 0A_0x99 3F
0x9A Rx/Tx 0A_0x9A 3F
0x9B Rx/Tx 0A_0x9B 00
0x0 Rx/Tx 0B_0x00 00
0x1 Rx/Tx 0B_0x01 80
0x2 Rx/Tx 0B_0x02 DC
0x3 Rx/Tx 0B_0x03 00
0x4 Rx/Tx 0B_0x04 01
0x5 Rx/Tx 0B_0x05 01
0x6 Rx/Tx 0B_0x06 01
0x7 Rx/Tx 0B_0x07 01
0x8 Rx/Tx 0B_0x08 60
0x9 Rx/Tx 0B_0x09 00
0xA Rx/Tx 0B_0x0A 50
0xB Rx/Tx 0B_0x0B 6F
0xC Rx/Tx 0B_0x0C 08
0xD Rx/Tx 0B_0x0D B4
0xE Rx/Tx 0B_0x0E 93
0xF Rx/Tx 0B_0x0F 69
0x10 Rx/Tx 0B_0x10 3A
0x11 Rx/Tx 0B_0x11 20
0x12 Rx/Tx 0B_0x12 E0
0x13 Rx/Tx 0B_0x13 90
0x14 Rx/Tx 0B_0x14 00
0x15 Rx/Tx 0B_0x15 12
0x16 Rx/Tx 0B_0x16 7A
0x17 Rx/Tx 0B_0x17 36
0x18 Rx/Tx 0B_0x18 40
0x19 Rx/Tx 0B_0x19 20
0x1A Rx/Tx 0B_0x1A A0
0x1B Rx/Tx 0B_0x1B 03
0x1C Rx/Tx 0B_0x1C 90
0x1D Rx/Tx 0B_0x1D 00
0x1E Rx/Tx 0B_0x1E E9
0x1F Rx/Tx 0B_0x1F 55
0x20 Rx/Tx 0B_0x20 00
0x21 Rx/Tx 0B_0x21 00
0x22 Rx/Tx 0B_0x22 00
0x23 Rx/Tx 0B_0x23 40
0x24 Rx/Tx 0B_0x24 00
0x25 Rx/Tx 0B_0x25 00
0x26 Rx/Tx 0B_0x26 00
0x27 Rx/Tx 0B_0x27 1D
0x28 Rx/Tx 0B_0x28 46
0x29 Rx/Tx 0B_0x29 20
0x2A Rx/Tx 0B_0x2A 30
0x2B Rx/Tx 0B_0x2B 0F
0x2C Rx/Tx 0B_0x2C F2
0x2D Rx/Tx 0B_0x2D 04
0x2E Rx/Tx 0B_0x2E 00
0x2F Rx/Tx 0B_0x2F 36
0x30 Rx/Tx 0B_0x30 00
0x31 Rx/Tx 0B_0x31 20
0x32 Rx/Tx 0B_0x32 11
0x33 Rx/Tx 0B_0x33 88
0x34 Rx/Tx 0B_0x34 BF
0x35 Rx/Tx 0B_0x35 1F
0x36 Rx/Tx 0B_0x36 30
0x37 Rx/Tx 0B_0x37 00
0x38 Rx/Tx 0B_0x38 00
0x39 Rx/Tx 0B_0x39 00
0x3A Rx/Tx 0B_0x3A 00
0x3B Rx/Tx 0B_0x3B 3E
0x3C Rx/Tx 0B_0x3C 7D
0x3D Rx/Tx 0B_0x3D 35
0x3E Rx/Tx 0B_0x3E 43
0x3F Rx/Tx 0B_0x3F C7
0x40 Rx/Tx 0B_0x40 00
0x41 Rx/Tx 0B_0x41 01
0x42 Rx/Tx 0B_0x42 04
0x43 Rx/Tx 0B_0x43 10
0x44 Rx/Tx 0B_0x44 40
0x45 Rx/Tx 0B_0x45 08
0x46 Rx/Tx 0B_0x46 02
0x47 Rx/Tx 0B_0x47 80
0x48 Rx/Tx 0B_0x48 03
0x49 Rx/Tx 0B_0x49 0C
0x4A Rx/Tx 0B_0x4A 30
0x4B Rx/Tx 0B_0x4B 41
0x4C Rx/Tx 0B_0x4C 50
0x4D Rx/Tx 0B_0x4D C0
0x4E Rx/Tx 0B_0x4E 60
0x4F Rx/Tx 0B_0x4F 90
0x50 Rx/Tx 0B_0x50 88
0x51 Rx/Tx 0B_0x51 82
0x52 Rx/Tx 0B_0x52 A0
0x53 Rx/Tx 0B_0x53 46
0x54 Rx/Tx 0B_0x54 52
0x55 Rx/Tx 0B_0x55 8C
0x56 Rx/Tx 0B_0x56 B0
0x57 Rx/Tx 0B_0x57 C8
0x58 Rx/Tx 0B_0x58 57
0x59 Rx/Tx 0B_0x59 5D
0x5A Rx/Tx 0B_0x5A 69
0x5B Rx/Tx 0B_0x5B 75
0x5C Rx/Tx 0B_0x5C D5
0x5D Rx/Tx 0B_0x5D 99
0x5E Rx/Tx 0B_0x5E 96
0x5F Rx/Tx 0B_0x5F A5
0x60 Rx/Tx 0B_0x60 00
0x61 Rx/Tx 0B_0x61 00
0x62 Rx/Tx 0B_0x62 00
0x63 Rx/Tx 0B_0x63 00
0x64 Rx/Tx 0B_0x64 00
0x65 Rx/Tx 0B_0x65 00
0x66 Rx/Tx 0B_0x66 00
0x67 Rx/Tx 0B_0x67 20
0x68 Rx/Tx 0B_0x68 00
0x69 Rx/Tx 0B_0x69 0A
0x6A Rx/Tx 0B_0x6A 22
0x6B Rx/Tx 0B_0x6B 40
0x6C Rx/Tx 0B_0x6C 00
0x6D Rx/Tx 0B_0x6D 00
0x6E Rx/Tx 0B_0x6E 00
0x6F Rx/Tx 0B_0x6F 00
0x70 Rx/Tx 0B_0x70 03
0x71 Rx/Tx 0B_0x71 20
0x72 Rx/Tx 0B_0x72 00
0x73 Rx/Tx 0B_0x73 00
0x74 Rx/Tx 0B_0x74 00
0x75 Rx/Tx 0B_0x75 00
0x76 Rx/Tx 0B_0x76 22
0x77 Rx/Tx 0B_0x77 1A
0x78 Rx/Tx 0B_0x78 30
0x79 Rx/Tx 0B_0x79 10
0x7A Rx/Tx 0B_0x7A 00
0x7B Rx/Tx 0B_0x7B 00
0x7C Rx/Tx 0B_0x7C 00
0x7D Rx/Tx 0B_0x7D 48
0x7E Rx/Tx 0B_0x7E 13
0x7F Rx/Tx 0B_0x7F 3A
0x80 Rx/Tx 0B_0x80 04
0x81 Rx/Tx 0B_0x81 E4
0x82 Rx/Tx 0B_0x82 00
0x83 Rx/Tx 0B_0x83 00
0x84 Rx/Tx 0B_0x84 10
0x85 Rx/Tx 0B_0x85 00
0x86 Rx/Tx 0B_0x86 00
0x87 Rx/Tx 0B_0x87 00
0x88 Rx/Tx 0B_0x88 00
0x89 Rx/Tx 0B_0x89 00
0x8A Rx/Tx 0B_0x8A 01
0x8B Rx/Tx 0B_0x8B 00
0x8C Rx/Tx 0B_0x8C 00
0x8D Rx/Tx 0B_0x8D 02
0x8E Rx/Tx 0B_0x8E 1C
0x8F Rx/Tx 0B_0x8F 00
0x90 Rx/Tx 0B_0x90 00
0x91 Rx/Tx 0B_0x91 00
0x92 Rx/Tx 0B_0x92 00
0x93 Rx/Tx 0B_0x93 00
0x94 Rx/Tx 0B_0x94 00
0x95 Rx/Tx 0B_0x95 00
0x96 Rx/Tx 0B_0x96 04
0x97 Rx/Tx 0B_0x97 00
0x98 Rx/Tx 0B_0x98 0C
0x99 Rx/Tx 0B_0x99 3F
0x9A Rx/Tx 0B_0x9A 3F
0x9B Rx/Tx 0B_0x9B 00
0x0 Rx/Tx 1A_0x00 00
0x1 Rx/Tx 1A_0x01 80
0x2 Rx/Tx 1A_0x02 DC
0x3 Rx/Tx 1A_0x03 00
0x4 Rx/Tx 1A_0x04 01
0x5 Rx/Tx 1A_0x05 01
0x6 Rx/Tx 1A_0x06 01
0x7 Rx/Tx 1A_0x07 01
0x8 Rx/Tx 1A_0x08 60
0x9 Rx/Tx 1A_0x09 00
0xA Rx/Tx 1A_0x0A 50
0xB Rx/Tx 1A_0x0B 6F
0xC Rx/Tx 1A_0x0C 08
0xD Rx/Tx 1A_0x0D B4
0xE Rx/Tx 1A_0x0E 93
0xF Rx/Tx 1A_0x0F 69
0x10 Rx/Tx 1A_0x10 3A
0x11 Rx/Tx 1A_0x11 20
0x12 Rx/Tx 1A_0x12 E0
0x13 Rx/Tx 1A_0x13 90
0x14 Rx/Tx 1A_0x14 00
0x15 Rx/Tx 1A_0x15 12
0x16 Rx/Tx 1A_0x16 7A
0x17 Rx/Tx 1A_0x17 36
0x18 Rx/Tx 1A_0x18 40
0x19 Rx/Tx 1A_0x19 20
0x1A Rx/Tx 1A_0x1A A0
0x1B Rx/Tx 1A_0x1B 03
0x1C Rx/Tx 1A_0x1C 90
0x1D Rx/Tx 1A_0x1D 00
0x1E Rx/Tx 1A_0x1E E9
0x1F Rx/Tx 1A_0x1F 55
0x20 Rx/Tx 1A_0x20 00
0x21 Rx/Tx 1A_0x21 00
0x22 Rx/Tx 1A_0x22 00
0x23 Rx/Tx 1A_0x23 40
0x24 Rx/Tx 1A_0x24 00
0x25 Rx/Tx 1A_0x25 00
0x26 Rx/Tx 1A_0x26 00
0x27 Rx/Tx 1A_0x27 27
0x28 Rx/Tx 1A_0x28 40
0x29 Rx/Tx 1A_0x29 20
0x2A Rx/Tx 1A_0x2A 30
0x2B Rx/Tx 1A_0x2B 0F
0x2C Rx/Tx 1A_0x2C F2
0x2D Rx/Tx 1A_0x2D 04
0x2E Rx/Tx 1A_0x2E 00
0x2F Rx/Tx 1A_0x2F 36
0x30 Rx/Tx 1A_0x30 00
0x31 Rx/Tx 1A_0x31 20
0x32 Rx/Tx 1A_0x32 11
0x33 Rx/Tx 1A_0x33 88
0x34 Rx/Tx 1A_0x34 BF
0x35 Rx/Tx 1A_0x35 1F
0x36 Rx/Tx 1A_0x36 30
0x37 Rx/Tx 1A_0x37 00
0x38 Rx/Tx 1A_0x38 00
0x39 Rx/Tx 1A_0x39 00
0x3A Rx/Tx 1A_0x3A 00
0x3B Rx/Tx 1A_0x3B 3E
0x3C Rx/Tx 1A_0x3C 7E
0x3D Rx/Tx 1A_0x3D 35
0x3E Rx/Tx 1A_0x3E 43
0x3F Rx/Tx 1A_0x3F C7
0x40 Rx/Tx 1A_0x40 00
0x41 Rx/Tx 1A_0x41 01
0x42 Rx/Tx 1A_0x42 04
0x43 Rx/Tx 1A_0x43 10
0x44 Rx/Tx 1A_0x44 40
0x45 Rx/Tx 1A_0x45 08
0x46 Rx/Tx 1A_0x46 02
0x47 Rx/Tx 1A_0x47 80
0x48 Rx/Tx 1A_0x48 03
0x49 Rx/Tx 1A_0x49 0C
0x4A Rx/Tx 1A_0x4A 30
0x4B Rx/Tx 1A_0x4B 41
0x4C Rx/Tx 1A_0x4C 50
0x4D Rx/Tx 1A_0x4D C0
0x4E Rx/Tx 1A_0x4E 60
0x4F Rx/Tx 1A_0x4F 90
0x50 Rx/Tx 1A_0x50 88
0x51 Rx/Tx 1A_0x51 82
0x52 Rx/Tx 1A_0x52 A0
0x53 Rx/Tx 1A_0x53 46
0x54 Rx/Tx 1A_0x54 52
0x55 Rx/Tx 1A_0x55 8C
0x56 Rx/Tx 1A_0x56 B0
0x57 Rx/Tx 1A_0x57 C8
0x58 Rx/Tx 1A_0x58 57
0x59 Rx/Tx 1A_0x59 5D
0x5A Rx/Tx 1A_0x5A 69
0x5B Rx/Tx 1A_0x5B 75
0x5C Rx/Tx 1A_0x5C D5
0x5D Rx/Tx 1A_0x5D 99
0x5E Rx/Tx 1A_0x5E 96
0x5F Rx/Tx 1A_0x5F A5
0x60 Rx/Tx 1A_0x60 00
0x61 Rx/Tx 1A_0x61 00
0x62 Rx/Tx 1A_0x62 00
0x63 Rx/Tx 1A_0x63 00
0x64 Rx/Tx 1A_0x64 00
0x65 Rx/Tx 1A_0x65 00
0x66 Rx/Tx 1A_0x66 00
0x67 Rx/Tx 1A_0x67 20
0x68 Rx/Tx 1A_0x68 00
0x69 Rx/Tx 1A_0x69 0A
0x6A Rx/Tx 1A_0x6A 22
0x6B Rx/Tx 1A_0x6B 40
0x6C Rx/Tx 1A_0x6C 00
0x6D Rx/Tx 1A_0x6D 00
0x6E Rx/Tx 1A_0x6E 00
0x6F Rx/Tx 1A_0x6F 00
0x70 Rx/Tx 1A_0x70 03
0x71 Rx/Tx 1A_0x71 20
0x72 Rx/Tx 1A_0x72 00
0x73 Rx/Tx 1A_0x73 00
0x74 Rx/Tx 1A_0x74 00
0x75 Rx/Tx 1A_0x75 00
0x76 Rx/Tx 1A_0x76 22
0x77 Rx/Tx 1A_0x77 1A
0x78 Rx/Tx 1A_0x78 30
0x79 Rx/Tx 1A_0x79 10
0x7A Rx/Tx 1A_0x7A 00
0x7B Rx/Tx 1A_0x7B 00
0x7C Rx/Tx 1A_0x7C 00
0x7D Rx/Tx 1A_0x7D 48
0x7E Rx/Tx 1A_0x7E 13
0x7F Rx/Tx 1A_0x7F 3A
0x80 Rx/Tx 1A_0x80 05
0x81 Rx/Tx 1A_0x81 E4
0x82 Rx/Tx 1A_0x82 00
0x83 Rx/Tx 1A_0x83 00
0x84 Rx/Tx 1A_0x84 00
0x85 Rx/Tx 1A_0x85 00
0x86 Rx/Tx 1A_0x86 00
0x87 Rx/Tx 1A_0x87 00
0x88 Rx/Tx 1A_0x88 00
0x89 Rx/Tx 1A_0x89 00
0x8A Rx/Tx 1A_0x8A 5F
0x8B Rx/Tx 1A_0x8B 00
0x8C Rx/Tx 1A_0x8C 00
0x8D Rx/Tx 1A_0x8D 02
0x8E Rx/Tx 1A_0x8E 1C
0x8F Rx/Tx 1A_0x8F 00
0x90 Rx/Tx 1A_0x90 00
0x91 Rx/Tx 1A_0x91 00
0x92 Rx/Tx 1A_0x92 00
0x93 Rx/Tx 1A_0x93 00
0x94 Rx/Tx 1A_0x94 00
0x95 Rx/Tx 1A_0x95 00
0x96 Rx/Tx 1A_0x96 04
0x97 Rx/Tx 1A_0x97 00
0x98 Rx/Tx 1A_0x98 0C
0x99 Rx/Tx 1A_0x99 3F
0x9A Rx/Tx 1A_0x9A 3F
0x9B Rx/Tx 1A_0x9B 00
0x0 Rx/Tx 1B_0x00 00
0x1 Rx/Tx 1B_0x01 80
0x2 Rx/Tx 1B_0x02 04
0x3 Rx/Tx 1B_0x03 00
0x4 Rx/Tx 1B_0x04 01
0x5 Rx/Tx 1B_0x05 01
0x6 Rx/Tx 1B_0x06 01
0x7 Rx/Tx 1B_0x07 01
0x8 Rx/Tx 1B_0x08 60
0x9 Rx/Tx 1B_0x09 00
0xA Rx/Tx 1B_0x0A 50
0xB Rx/Tx 1B_0x0B 6F
0xC Rx/Tx 1B_0x0C 08
0xD Rx/Tx 1B_0x0D B4
0xE Rx/Tx 1B_0x0E 93
0xF Rx/Tx 1B_0x0F 69
0x10 Rx/Tx 1B_0x10 3A
0x11 Rx/Tx 1B_0x11 20
0x12 Rx/Tx 1B_0x12 E0
0x13 Rx/Tx 1B_0x13 90
0x14 Rx/Tx 1B_0x14 00
0x15 Rx/Tx 1B_0x15 12
0x16 Rx/Tx 1B_0x16 7A
0x17 Rx/Tx 1B_0x17 36
0x18 Rx/Tx 1B_0x18 40
0x19 Rx/Tx 1B_0x19 20
0x1A Rx/Tx 1B_0x1A A0
0x1B Rx/Tx 1B_0x1B 03
0x1C Rx/Tx 1B_0x1C 90
0x1D Rx/Tx 1B_0x1D 00
0x1E Rx/Tx 1B_0x1E E9
0x1F Rx/Tx 1B_0x1F 55
0x20 Rx/Tx 1B_0x20 00
0x21 Rx/Tx 1B_0x21 00
0x22 Rx/Tx 1B_0x22 00
0x23 Rx/Tx 1B_0x23 40
0x24 Rx/Tx 1B_0x24 40
0x25 Rx/Tx 1B_0x25 00
0x26 Rx/Tx 1B_0x26 00
0x27 Rx/Tx 1B_0x27 00
0x28 Rx/Tx 1B_0x28 00
0x29 Rx/Tx 1B_0x29 00
0x2A Rx/Tx 1B_0x2A 30
0x2B Rx/Tx 1B_0x2B 0F
0x2C Rx/Tx 1B_0x2C F2
0x2D Rx/Tx 1B_0x2D 04
0x2E Rx/Tx 1B_0x2E 00
0x2F Rx/Tx 1B_0x2F 36
0x30 Rx/Tx 1B_0x30 00
0x31 Rx/Tx 1B_0x31 20
0x32 Rx/Tx 1B_0x32 11
0x33 Rx/Tx 1B_0x33 88
0x34 Rx/Tx 1B_0x34 BF
0x35 Rx/Tx 1B_0x35 1F
0x36 Rx/Tx 1B_0x36 30
0x37 Rx/Tx 1B_0x37 1A
0x38 Rx/Tx 1B_0x38 00
0x39 Rx/Tx 1B_0x39 00
0x3A Rx/Tx 1B_0x3A 00
0x3B Rx/Tx 1B_0x3B 3E
0x3C Rx/Tx 1B_0x3C 7E
0x3D Rx/Tx 1B_0x3D 35
0x3E Rx/Tx 1B_0x3E 43
0x3F Rx/Tx 1B_0x3F C7
0x40 Rx/Tx 1B_0x40 00
0x41 Rx/Tx 1B_0x41 01
0x42 Rx/Tx 1B_0x42 04
0x43 Rx/Tx 1B_0x43 10
0x44 Rx/Tx 1B_0x44 40
0x45 Rx/Tx 1B_0x45 08
0x46 Rx/Tx 1B_0x46 02
0x47 Rx/Tx 1B_0x47 80
0x48 Rx/Tx 1B_0x48 03
0x49 Rx/Tx 1B_0x49 0C
0x4A Rx/Tx 1B_0x4A 30
0x4B Rx/Tx 1B_0x4B 41
0x4C Rx/Tx 1B_0x4C 50
0x4D Rx/Tx 1B_0x4D C0
0x4E Rx/Tx 1B_0x4E 60
0x4F Rx/Tx 1B_0x4F 90
0x50 Rx/Tx 1B_0x50 88
0x51 Rx/Tx 1B_0x51 82
0x52 Rx/Tx 1B_0x52 A0
0x53 Rx/Tx 1B_0x53 46
0x54 Rx/Tx 1B_0x54 52
0x55 Rx/Tx 1B_0x55 8C
0x56 Rx/Tx 1B_0x56 B0
0x57 Rx/Tx 1B_0x57 C8
0x58 Rx/Tx 1B_0x58 57
0x59 Rx/Tx 1B_0x59 5D
0x5A Rx/Tx 1B_0x5A 69
0x5B Rx/Tx 1B_0x5B 75
0x5C Rx/Tx 1B_0x5C D5
0x5D Rx/Tx 1B_0x5D 99
0x5E Rx/Tx 1B_0x5E 96
0x5F Rx/Tx 1B_0x5F A5
0x60 Rx/Tx 1B_0x60 00
0x61 Rx/Tx 1B_0x61 00
0x62 Rx/Tx 1B_0x62 00
0x63 Rx/Tx 1B_0x63 00
0x64 Rx/Tx 1B_0x64 00
0x65 Rx/Tx 1B_0x65 00
0x66 Rx/Tx 1B_0x66 00
0x67 Rx/Tx 1B_0x67 20
0x68 Rx/Tx 1B_0x68 00
0x69 Rx/Tx 1B_0x69 0A
0x6A Rx/Tx 1B_0x6A 22
0x6B Rx/Tx 1B_0x6B 40
0x6C Rx/Tx 1B_0x6C 00
0x6D Rx/Tx 1B_0x6D 00
0x6E Rx/Tx 1B_0x6E 00
0x6F Rx/Tx 1B_0x6F 00
0x70 Rx/Tx 1B_0x70 03
0x71 Rx/Tx 1B_0x71 20
0x72 Rx/Tx 1B_0x72 00
0x73 Rx/Tx 1B_0x73 00
0x74 Rx/Tx 1B_0x74 00
0x75 Rx/Tx 1B_0x75 00
0x76 Rx/Tx 1B_0x76 22
0x77 Rx/Tx 1B_0x77 1A
0x78 Rx/Tx 1B_0x78 20
0x79 Rx/Tx 1B_0x79 10
0x7A Rx/Tx 1B_0x7A 00
0x7B Rx/Tx 1B_0x7B 00
0x7C Rx/Tx 1B_0x7C 00
0x7D Rx/Tx 1B_0x7D 48
0x7E Rx/Tx 1B_0x7E 13
0x7F Rx/Tx 1B_0x7F 3A
0x80 Rx/Tx 1B_0x80 00
0x81 Rx/Tx 1B_0x81 E4
0x82 Rx/Tx 1B_0x82 00
0x83 Rx/Tx 1B_0x83 07
0x84 Rx/Tx 1B_0x84 FF
0x85 Rx/Tx 1B_0x85 00
0x86 Rx/Tx 1B_0x86 00
0x87 Rx/Tx 1B_0x87 00
0x88 Rx/Tx 1B_0x88 00
0x89 Rx/Tx 1B_0x89 02
0x8A Rx/Tx 1B_0x8A AD
0x8B Rx/Tx 1B_0x8B 00
0x8C Rx/Tx 1B_0x8C 00
0x8D Rx/Tx 1B_0x8D 02
0x8E Rx/Tx 1B_0x8E 1C
0x8F Rx/Tx 1B_0x8F 50
0x90 Rx/Tx 1B_0x90 00
0x91 Rx/Tx 1B_0x91 00
0x92 Rx/Tx 1B_0x92 00
0x93 Rx/Tx 1B_0x93 00
0x94 Rx/Tx 1B_0x94 00
0x95 Rx/Tx 1B_0x95 00
0x96 Rx/Tx 1B_0x96 04
0x97 Rx/Tx 1B_0x97 00
0x98 Rx/Tx 1B_0x98 0C
0x99 Rx/Tx 1B_0x99 3F
0x9A Rx/Tx 1B_0x9A 3F
0x9B Rx/Tx 1B_0x9B 00
0x0 Rx/Tx 2A_0x00 00
0x1 Rx/Tx 2A_0x01 80
0x2 Rx/Tx 2A_0x02 00
0x3 Rx/Tx 2A_0x03 00
0x4 Rx/Tx 2A_0x04 01
0x5 Rx/Tx 2A_0x05 01
0x6 Rx/Tx 2A_0x06 01
0x7 Rx/Tx 2A_0x07 01
0x8 Rx/Tx 2A_0x08 60
0x9 Rx/Tx 2A_0x09 00
0xA Rx/Tx 2A_0x0A 50
0xB Rx/Tx 2A_0x0B 6F
0xC Rx/Tx 2A_0x0C 08
0xD Rx/Tx 2A_0x0D B4
0xE Rx/Tx 2A_0x0E 93
0xF Rx/Tx 2A_0x0F 69
0x10 Rx/Tx 2A_0x10 3A
0x11 Rx/Tx 2A_0x11 20
0x12 Rx/Tx 2A_0x12 E0
0x13 Rx/Tx 2A_0x13 90
0x14 Rx/Tx 2A_0x14 00
0x15 Rx/Tx 2A_0x15 12
0x16 Rx/Tx 2A_0x16 7A
0x17 Rx/Tx 2A_0x17 36
0x18 Rx/Tx 2A_0x18 40
0x19 Rx/Tx 2A_0x19 20
0x1A Rx/Tx 2A_0x1A A0
0x1B Rx/Tx 2A_0x1B 03
0x1C Rx/Tx 2A_0x1C 90
0x1D Rx/Tx 2A_0x1D 00
0x1E Rx/Tx 2A_0x1E E9
0x1F Rx/Tx 2A_0x1F 55
0x20 Rx/Tx 2A_0x20 00
0x21 Rx/Tx 2A_0x21 00
0x22 Rx/Tx 2A_0x22 00
0x23 Rx/Tx 2A_0x23 40
0x24 Rx/Tx 2A_0x24 40
0x25 Rx/Tx 2A_0x25 00
0x26 Rx/Tx 2A_0x26 00
0x27 Rx/Tx 2A_0x27 00
0x28 Rx/Tx 2A_0x28 00
0x29 Rx/Tx 2A_0x29 00
0x2A Rx/Tx 2A_0x2A 30
0x2B Rx/Tx 2A_0x2B 0F
0x2C Rx/Tx 2A_0x2C F2
0x2D Rx/Tx 2A_0x2D 04
0x2E Rx/Tx 2A_0x2E 00
0x2F Rx/Tx 2A_0x2F 36
0x30 Rx/Tx 2A_0x30 00
0x31 Rx/Tx 2A_0x31 20
0x32 Rx/Tx 2A_0x32 11
0x33 Rx/Tx 2A_0x33 88
0x34 Rx/Tx 2A_0x34 BF
0x35 Rx/Tx 2A_0x35 1F
0x36 Rx/Tx 2A_0x36 30
0x37 Rx/Tx 2A_0x37 00
0x38 Rx/Tx 2A_0x38 00
0x39 Rx/Tx 2A_0x39 00
0x3A Rx/Tx 2A_0x3A 00
0x3B Rx/Tx 2A_0x3B 3D
0x3C Rx/Tx 2A_0x3C 31
0x3D Rx/Tx 2A_0x3D 35
0x3E Rx/Tx 2A_0x3E 43
0x3F Rx/Tx 2A_0x3F C7
0x40 Rx/Tx 2A_0x40 00
0x41 Rx/Tx 2A_0x41 01
0x42 Rx/Tx 2A_0x42 04
0x43 Rx/Tx 2A_0x43 10
0x44 Rx/Tx 2A_0x44 40
0x45 Rx/Tx 2A_0x45 08
0x46 Rx/Tx 2A_0x46 02
0x47 Rx/Tx 2A_0x47 80
0x48 Rx/Tx 2A_0x48 03
0x49 Rx/Tx 2A_0x49 0C
0x4A Rx/Tx 2A_0x4A 30
0x4B Rx/Tx 2A_0x4B 41
0x4C Rx/Tx 2A_0x4C 50
0x4D Rx/Tx 2A_0x4D C0
0x4E Rx/Tx 2A_0x4E 60
0x4F Rx/Tx 2A_0x4F 90
0x50 Rx/Tx 2A_0x50 88
0x51 Rx/Tx 2A_0x51 82
0x52 Rx/Tx 2A_0x52 A0
0x53 Rx/Tx 2A_0x53 46
0x54 Rx/Tx 2A_0x54 52
0x55 Rx/Tx 2A_0x55 8C
0x56 Rx/Tx 2A_0x56 B0
0x57 Rx/Tx 2A_0x57 C8
0x58 Rx/Tx 2A_0x58 57
0x59 Rx/Tx 2A_0x59 5D
0x5A Rx/Tx 2A_0x5A 69
0x5B Rx/Tx 2A_0x5B 75
0x5C Rx/Tx 2A_0x5C D5
0x5D Rx/Tx 2A_0x5D 99
0x5E Rx/Tx 2A_0x5E 96
0x5F Rx/Tx 2A_0x5F A5
0x60 Rx/Tx 2A_0x60 00
0x61 Rx/Tx 2A_0x61 00
0x62 Rx/Tx 2A_0x62 00
0x63 Rx/Tx 2A_0x63 00
0x64 Rx/Tx 2A_0x64 00
0x65 Rx/Tx 2A_0x65 00
0x66 Rx/Tx 2A_0x66 00
0x67 Rx/Tx 2A_0x67 20
0x68 Rx/Tx 2A_0x68 00
0x69 Rx/Tx 2A_0x69 0A
0x6A Rx/Tx 2A_0x6A 22
0x6B Rx/Tx 2A_0x6B 40
0x6C Rx/Tx 2A_0x6C 00
0x6D Rx/Tx 2A_0x6D 00
0x6E Rx/Tx 2A_0x6E 00
0x6F Rx/Tx 2A_0x6F 00
0x70 Rx/Tx 2A_0x70 03
0x71 Rx/Tx 2A_0x71 20
0x72 Rx/Tx 2A_0x72 00
0x73 Rx/Tx 2A_0x73 00
0x74 Rx/Tx 2A_0x74 00
0x75 Rx/Tx 2A_0x75 00
0x76 Rx/Tx 2A_0x76 22
0x77 Rx/Tx 2A_0x77 1A
0x78 Rx/Tx 2A_0x78 20
0x79 Rx/Tx 2A_0x79 10
0x7A Rx/Tx 2A_0x7A 00
0x7B Rx/Tx 2A_0x7B 00
0x7C Rx/Tx 2A_0x7C 00
0x7D Rx/Tx 2A_0x7D 48
0x7E Rx/Tx 2A_0x7E 13
0x7F Rx/Tx 2A_0x7F 3A
0x80 Rx/Tx 2A_0x80 00
0x81 Rx/Tx 2A_0x81 E4
0x82 Rx/Tx 2A_0x82 00
0x83 Rx/Tx 2A_0x83 00
0x84 Rx/Tx 2A_0x84 2A
0x85 Rx/Tx 2A_0x85 00
0x86 Rx/Tx 2A_0x86 00
0x87 Rx/Tx 2A_0x87 00
0x88 Rx/Tx 2A_0x88 00
0x89 Rx/Tx 2A_0x89 00
0x8A Rx/Tx 2A_0x8A 0C
0x8B Rx/Tx 2A_0x8B 00
0x8C Rx/Tx 2A_0x8C 00
0x8D Rx/Tx 2A_0x8D 02
0x8E Rx/Tx 2A_0x8E 1C
0x8F Rx/Tx 2A_0x8F 60
0x90 Rx/Tx 2A_0x90 00
0x91 Rx/Tx 2A_0x91 00
0x92 Rx/Tx 2A_0x92 00
0x93 Rx/Tx 2A_0x93 00
0x94 Rx/Tx 2A_0x94 00
0x95 Rx/Tx 2A_0x95 00
0x96 Rx/Tx 2A_0x96 04
0x97 Rx/Tx 2A_0x97 00
0x98 Rx/Tx 2A_0x98 0C
0x99 Rx/Tx 2A_0x99 3F
0x9A Rx/Tx 2A_0x9A 3F
0x9B Rx/Tx 2A_0x9B 00
0x0 Rx/Tx 2B_0x00 00
0x1 Rx/Tx 2B_0x01 80
0x2 Rx/Tx 2B_0x02 84
0x3 Rx/Tx 2B_0x03 00
0x4 Rx/Tx 2B_0x04 01
0x5 Rx/Tx 2B_0x05 01
0x6 Rx/Tx 2B_0x06 01
0x7 Rx/Tx 2B_0x07 01
0x8 Rx/Tx 2B_0x08 60
0x9 Rx/Tx 2B_0x09 00
0xA Rx/Tx 2B_0x0A 50
0xB Rx/Tx 2B_0x0B 6F
0xC Rx/Tx 2B_0x0C 08
0xD Rx/Tx 2B_0x0D B4
0xE Rx/Tx 2B_0x0E 93
0xF Rx/Tx 2B_0x0F 69
0x10 Rx/Tx 2B_0x10 3A
0x11 Rx/Tx 2B_0x11 20
0x12 Rx/Tx 2B_0x12 E0
0x13 Rx/Tx 2B_0x13 90
0x14 Rx/Tx 2B_0x14 00
0x15 Rx/Tx 2B_0x15 12
0x16 Rx/Tx 2B_0x16 7A
0x17 Rx/Tx 2B_0x17 36
0x18 Rx/Tx 2B_0x18 40
0x19 Rx/Tx 2B_0x19 20
0x1A Rx/Tx 2B_0x1A A0
0x1B Rx/Tx 2B_0x1B 03
0x1C Rx/Tx 2B_0x1C 90
0x1D Rx/Tx 2B_0x1D 00
0x1E Rx/Tx 2B_0x1E E9
0x1F Rx/Tx 2B_0x1F 55
0x20 Rx/Tx 2B_0x20 00
0x21 Rx/Tx 2B_0x21 00
0x22 Rx/Tx 2B_0x22 00
0x23 Rx/Tx 2B_0x23 40
0x24 Rx/Tx 2B_0x24 40
0x25 Rx/Tx 2B_0x25 00
0x26 Rx/Tx 2B_0x26 00
0x27 Rx/Tx 2B_0x27 00
0x28 Rx/Tx 2B_0x28 00
0x29 Rx/Tx 2B_0x29 00
0x2A Rx/Tx 2B_0x2A 30
0x2B Rx/Tx 2B_0x2B 0F
0x2C Rx/Tx 2B_0x2C F2
0x2D Rx/Tx 2B_0x2D 04
0x2E Rx/Tx 2B_0x2E 00
0x2F Rx/Tx 2B_0x2F 36
0x30 Rx/Tx 2B_0x30 00
0x31 Rx/Tx 2B_0x31 20
0x32 Rx/Tx 2B_0x32 11
0x33 Rx/Tx 2B_0x33 88
0x34 Rx/Tx 2B_0x34 BF
0x35 Rx/Tx 2B_0x35 1F
0x36 Rx/Tx 2B_0x36 30
0x37 Rx/Tx 2B_0x37 0E
0x38 Rx/Tx 2B_0x38 00
0x39 Rx/Tx 2B_0x39 00
0x3A Rx/Tx 2B_0x3A 00
0x3B Rx/Tx 2B_0x3B 3D
0x3C Rx/Tx 2B_0x3C 82
0x3D Rx/Tx 2B_0x3D 35
0x3E Rx/Tx 2B_0x3E 43
0x3F Rx/Tx 2B_0x3F C7
0x40 Rx/Tx 2B_0x40 00
0x41 Rx/Tx 2B_0x41 01
0x42 Rx/Tx 2B_0x42 04
0x43 Rx/Tx 2B_0x43 10
0x44 Rx/Tx 2B_0x44 40
0x45 Rx/Tx 2B_0x45 08
0x46 Rx/Tx 2B_0x46 02
0x47 Rx/Tx 2B_0x47 80
0x48 Rx/Tx 2B_0x48 03
0x49 Rx/Tx 2B_0x49 0C
0x4A Rx/Tx 2B_0x4A 30
0x4B Rx/Tx 2B_0x4B 41
0x4C Rx/Tx 2B_0x4C 50
0x4D Rx/Tx 2B_0x4D C0
0x4E Rx/Tx 2B_0x4E 60
0x4F Rx/Tx 2B_0x4F 90
0x50 Rx/Tx 2B_0x50 88
0x51 Rx/Tx 2B_0x51 82
0x52 Rx/Tx 2B_0x52 A0
0x53 Rx/Tx 2B_0x53 46
0x54 Rx/Tx 2B_0x54 52
0x55 Rx/Tx 2B_0x55 8C
0x56 Rx/Tx 2B_0x56 B0
0x57 Rx/Tx 2B_0x57 C8
0x58 Rx/Tx 2B_0x58 57
0x59 Rx/Tx 2B_0x59 5D
0x5A Rx/Tx 2B_0x5A 69
0x5B Rx/Tx 2B_0x5B 75
0x5C Rx/Tx 2B_0x5C D5
0x5D Rx/Tx 2B_0x5D 99
0x5E Rx/Tx 2B_0x5E 96
0x5F Rx/Tx 2B_0x5F A5
0x60 Rx/Tx 2B_0x60 00
0x61 Rx/Tx 2B_0x61 00
0x62 Rx/Tx 2B_0x62 00
0x63 Rx/Tx 2B_0x63 00
0x64 Rx/Tx 2B_0x64 00
0x65 Rx/Tx 2B_0x65 00
0x66 Rx/Tx 2B_0x66 00
0x67 Rx/Tx 2B_0x67 20
0x68 Rx/Tx 2B_0x68 00
0x69 Rx/Tx 2B_0x69 0A
0x6A Rx/Tx 2B_0x6A 22
0x6B Rx/Tx 2B_0x6B 40
0x6C Rx/Tx 2B_0x6C 00
0x6D Rx/Tx 2B_0x6D 00
0x6E Rx/Tx 2B_0x6E 00
0x6F Rx/Tx 2B_0x6F 00
0x70 Rx/Tx 2B_0x70 03
0x71 Rx/Tx 2B_0x71 20
0x72 Rx/Tx 2B_0x72 00
0x73 Rx/Tx 2B_0x73 00
0x74 Rx/Tx 2B_0x74 00
0x75 Rx/Tx 2B_0x75 00
0x76 Rx/Tx 2B_0x76 22
0x77 Rx/Tx 2B_0x77 1A
0x78 Rx/Tx 2B_0x78 20
0x79 Rx/Tx 2B_0x79 10
0x7A Rx/Tx 2B_0x7A 00
0x7B Rx/Tx 2B_0x7B 00
0x7C Rx/Tx 2B_0x7C 00
0x7D Rx/Tx 2B_0x7D 48
0x7E Rx/Tx 2B_0x7E 13
0x7F Rx/Tx 2B_0x7F 3A
0x80 Rx/Tx 2B_0x80 00
0x81 Rx/Tx 2B_0x81 E4
0x82 Rx/Tx 2B_0x82 00
0x83 Rx/Tx 2B_0x83 00
0x84 Rx/Tx 2B_0x84 00
0x85 Rx/Tx 2B_0x85 04
0x86 Rx/Tx 2B_0x86 20
0x87 Rx/Tx 2B_0x87 00
0x88 Rx/Tx 2B_0x88 00
0x89 Rx/Tx 2B_0x89 00
0x8A Rx/Tx 2B_0x8A 00
0x8B Rx/Tx 2B_0x8B 00
0x8C Rx/Tx 2B_0x8C 00
0x8D Rx/Tx 2B_0x8D 02
0x8E Rx/Tx 2B_0x8E 1C
0x8F Rx/Tx 2B_0x8F 00
0x90 Rx/Tx 2B_0x90 00
0x91 Rx/Tx 2B_0x91 00
0x92 Rx/Tx 2B_0x92 00
0x93 Rx/Tx 2B_0x93 00
0x94 Rx/Tx 2B_0x94 00
0x95 Rx/Tx 2B_0x95 00
0x96 Rx/Tx 2B_0x96 04
0x97 Rx/Tx 2B_0x97 00
0x98 Rx/Tx 2B_0x98 0C
0x99 Rx/Tx 2B_0x99 3F
0x9A Rx/Tx 2B_0x9A 3F
0x9B Rx/Tx 2B_0x9B 00
0x0 Rx/Tx 3A_0x00 00
0x1 Rx/Tx 3A_0x01 80
0x2 Rx/Tx 3A_0x02 DC
0x3 Rx/Tx 3A_0x03 00
0x4 Rx/Tx 3A_0x04 01
0x5 Rx/Tx 3A_0x05 01
0x6 Rx/Tx 3A_0x06 01
0x7 Rx/Tx 3A_0x07 01
0x8 Rx/Tx 3A_0x08 60
0x9 Rx/Tx 3A_0x09 00
0xA Rx/Tx 3A_0x0A 50
0xB Rx/Tx 3A_0x0B 6F
0xC Rx/Tx 3A_0x0C 08
0xD Rx/Tx 3A_0x0D B4
0xE Rx/Tx 3A_0x0E 93
0xF Rx/Tx 3A_0x0F 69
0x10 Rx/Tx 3A_0x10 3A
0x11 Rx/Tx 3A_0x11 20
0x12 Rx/Tx 3A_0x12 E0
0x13 Rx/Tx 3A_0x13 90
0x14 Rx/Tx 3A_0x14 00
0x15 Rx/Tx 3A_0x15 12
0x16 Rx/Tx 3A_0x16 7A
0x17 Rx/Tx 3A_0x17 36
0x18 Rx/Tx 3A_0x18 40
0x19 Rx/Tx 3A_0x19 20
0x1A Rx/Tx 3A_0x1A A0
0x1B Rx/Tx 3A_0x1B 03
0x1C Rx/Tx 3A_0x1C 90
0x1D Rx/Tx 3A_0x1D 00
0x1E Rx/Tx 3A_0x1E E9
0x1F Rx/Tx 3A_0x1F 55
0x20 Rx/Tx 3A_0x20 00
0x21 Rx/Tx 3A_0x21 00
0x22 Rx/Tx 3A_0x22 00
0x23 Rx/Tx 3A_0x23 40
0x24 Rx/Tx 3A_0x24 00
0x25 Rx/Tx 3A_0x25 00
0x26 Rx/Tx 3A_0x26 00
0x27 Rx/Tx 3A_0x27 27
0x28 Rx/Tx 3A_0x28 3E
0x29 Rx/Tx 3A_0x29 20
0x2A Rx/Tx 3A_0x2A 30
0x2B Rx/Tx 3A_0x2B 0F
0x2C Rx/Tx 3A_0x2C F2
0x2D Rx/Tx 3A_0x2D 04
0x2E Rx/Tx 3A_0x2E 00
0x2F Rx/Tx 3A_0x2F 36
0x30 Rx/Tx 3A_0x30 00
0x31 Rx/Tx 3A_0x31 20
0x32 Rx/Tx 3A_0x32 11
0x33 Rx/Tx 3A_0x33 88
0x34 Rx/Tx 3A_0x34 BF
0x35 Rx/Tx 3A_0x35 1F
0x36 Rx/Tx 3A_0x36 30
0x37 Rx/Tx 3A_0x37 00
0x38 Rx/Tx 3A_0x38 00
0x39 Rx/Tx 3A_0x39 00
0x3A Rx/Tx 3A_0x3A 00
0x3B Rx/Tx 3A_0x3B 3E
0x3C Rx/Tx 3A_0x3C 7D
0x3D Rx/Tx 3A_0x3D 35
0x3E Rx/Tx 3A_0x3E 43
0x3F Rx/Tx 3A_0x3F C7
0x40 Rx/Tx 3A_0x40 00
0x41 Rx/Tx 3A_0x41 01
0x42 Rx/Tx 3A_0x42 04
0x43 Rx/Tx 3A_0x43 10
0x44 Rx/Tx 3A_0x44 40
0x45 Rx/Tx 3A_0x45 08
0x46 Rx/Tx 3A_0x46 02
0x47 Rx/Tx 3A_0x47 80
0x48 Rx/Tx 3A_0x48 03
0x49 Rx/Tx 3A_0x49 0C
0x4A Rx/Tx 3A_0x4A 30
0x4B Rx/Tx 3A_0x4B 41
0x4C Rx/Tx 3A_0x4C 50
0x4D Rx/Tx 3A_0x4D C0
0x4E Rx/Tx 3A_0x4E 60
0x4F Rx/Tx 3A_0x4F 90
0x50 Rx/Tx 3A_0x50 88
0x51 Rx/Tx 3A_0x51 82
0x52 Rx/Tx 3A_0x52 A0
0x53 Rx/Tx 3A_0x53 46
0x54 Rx/Tx 3A_0x54 52
0x55 Rx/Tx 3A_0x55 8C
0x56 Rx/Tx 3A_0x56 B0
0x57 Rx/Tx 3A_0x57 C8
0x58 Rx/Tx 3A_0x58 57
0x59 Rx/Tx 3A_0x59 5D
0x5A Rx/Tx 3A_0x5A 69
0x5B Rx/Tx 3A_0x5B 75
0x5C Rx/Tx 3A_0x5C D5
0x5D Rx/Tx 3A_0x5D 99
0x5E Rx/Tx 3A_0x5E 96
0x5F Rx/Tx 3A_0x5F A5
0x60 Rx/Tx 3A_0x60 00
0x61 Rx/Tx 3A_0x61 00
0x62 Rx/Tx 3A_0x62 00
0x63 Rx/Tx 3A_0x63 00
0x64 Rx/Tx 3A_0x64 00
0x65 Rx/Tx 3A_0x65 00
0x66 Rx/Tx 3A_0x66 00
0x67 Rx/Tx 3A_0x67 20
0x68 Rx/Tx 3A_0x68 00
0x69 Rx/Tx 3A_0x69 0A
0x6A Rx/Tx 3A_0x6A 22
0x6B Rx/Tx 3A_0x6B 40
0x6C Rx/Tx 3A_0x6C 00
0x6D Rx/Tx 3A_0x6D 00
0x6E Rx/Tx 3A_0x6E 00
0x6F Rx/Tx 3A_0x6F 00
0x70 Rx/Tx 3A_0x70 03
0x71 Rx/Tx 3A_0x71 20
0x72 Rx/Tx 3A_0x72 00
0x73 Rx/Tx 3A_0x73 00
0x74 Rx/Tx 3A_0x74 00
0x75 Rx/Tx 3A_0x75 00
0x76 Rx/Tx 3A_0x76 22
0x77 Rx/Tx 3A_0x77 1A
0x78 Rx/Tx 3A_0x78 30
0x79 Rx/Tx 3A_0x79 10
0x7A Rx/Tx 3A_0x7A 00
0x7B Rx/Tx 3A_0x7B 00
0x7C Rx/Tx 3A_0x7C 00
0x7D Rx/Tx 3A_0x7D 48
0x7E Rx/Tx 3A_0x7E 13
0x7F Rx/Tx 3A_0x7F 3A
0x80 Rx/Tx 3A_0x80 03
0x81 Rx/Tx 3A_0x81 E4
0x82 Rx/Tx 3A_0x82 00
0x83 Rx/Tx 3A_0x83 00
0x84 Rx/Tx 3A_0x84 22
0x85 Rx/Tx 3A_0x85 00
0x86 Rx/Tx 3A_0x86 00
0x87 Rx/Tx 3A_0x87 00
0x88 Rx/Tx 3A_0x88 00
0x89 Rx/Tx 3A_0x89 00
0x8A Rx/Tx 3A_0x8A 01
0x8B Rx/Tx 3A_0x8B 00
0x8C Rx/Tx 3A_0x8C 00
0x8D Rx/Tx 3A_0x8D 02
0x8E Rx/Tx 3A_0x8E 1C
0x8F Rx/Tx 3A_0x8F 00
0x90 Rx/Tx 3A_0x90 00
0x91 Rx/Tx 3A_0x91 00
0x92 Rx/Tx 3A_0x92 00
0x93 Rx/Tx 3A_0x93 00
0x94 Rx/Tx 3A_0x94 00
0x95 Rx/Tx 3A_0x95 00
0x96 Rx/Tx 3A_0x96 04
0x97 Rx/Tx 3A_0x97 00
0x98 Rx/Tx 3A_0x98 0C
0x99 Rx/Tx 3A_0x99 3F
0x9A Rx/Tx 3A_0x9A 3F
0x9B Rx/Tx 3A_0x9B 00
0x0 Rx/Tx 3B_0x00 00
0x1 Rx/Tx 3B_0x01 80
0x2 Rx/Tx 3B_0x02 DC
0x3 Rx/Tx 3B_0x03 00
0x4 Rx/Tx 3B_0x04 01
0x5 Rx/Tx 3B_0x05 01
0x6 Rx/Tx 3B_0x06 01
0x7 Rx/Tx 3B_0x07 01
0x8 Rx/Tx 3B_0x08 60
0x9 Rx/Tx 3B_0x09 00
0xA Rx/Tx 3B_0x0A 50
0xB Rx/Tx 3B_0x0B 6F
0xC Rx/Tx 3B_0x0C 08
0xD Rx/Tx 3B_0x0D B4
0xE Rx/Tx 3B_0x0E 93
0xF Rx/Tx 3B_0x0F 69
0x10 Rx/Tx 3B_0x10 3A
0x11 Rx/Tx 3B_0x11 20
0x12 Rx/Tx 3B_0x12 E0
0x13 Rx/Tx 3B_0x13 90
0x14 Rx/Tx 3B_0x14 00
0x15 Rx/Tx 3B_0x15 12
0x16 Rx/Tx 3B_0x16 7A
0x17 Rx/Tx 3B_0x17 36
0x18 Rx/Tx 3B_0x18 40
0x19 Rx/Tx 3B_0x19 20
0x1A Rx/Tx 3B_0x1A A0
0x1B Rx/Tx 3B_0x1B 03
0x1C Rx/Tx 3B_0x1C 90
0x1D Rx/Tx 3B_0x1D 00
0x1E Rx/Tx 3B_0x1E E9
0x1F Rx/Tx 3B_0x1F 55
0x20 Rx/Tx 3B_0x20 00
0x21 Rx/Tx 3B_0x21 00
0x22 Rx/Tx 3B_0x22 00
0x23 Rx/Tx 3B_0x23 40
0x24 Rx/Tx 3B_0x24 00
0x25 Rx/Tx 3B_0x25 00
0x26 Rx/Tx 3B_0x26 00
0x27 Rx/Tx 3B_0x27 2C
0x28 Rx/Tx 3B_0x28 38
0x29 Rx/Tx 3B_0x29 00
0x2A Rx/Tx 3B_0x2A 30
0x2B Rx/Tx 3B_0x2B 0F
0x2C Rx/Tx 3B_0x2C F2
0x2D Rx/Tx 3B_0x2D 04
0x2E Rx/Tx 3B_0x2E 00
0x2F Rx/Tx 3B_0x2F 36
0x30 Rx/Tx 3B_0x30 00
0x31 Rx/Tx 3B_0x31 20
0x32 Rx/Tx 3B_0x32 11
0x33 Rx/Tx 3B_0x33 88
0x34 Rx/Tx 3B_0x34 BF
0x35 Rx/Tx 3B_0x35 1F
0x36 Rx/Tx 3B_0x36 30
0x37 Rx/Tx 3B_0x37 00
0x38 Rx/Tx 3B_0x38 00
0x39 Rx/Tx 3B_0x39 00
0x3A Rx/Tx 3B_0x3A 00
0x3B Rx/Tx 3B_0x3B 3E
0x3C Rx/Tx 3B_0x3C 7D
0x3D Rx/Tx 3B_0x3D 35
0x3E Rx/Tx 3B_0x3E 43
0x3F Rx/Tx 3B_0x3F C7
0x40 Rx/Tx 3B_0x40 00
0x41 Rx/Tx 3B_0x41 01
0x42 Rx/Tx 3B_0x42 04
0x43 Rx/Tx 3B_0x43 10
0x44 Rx/Tx 3B_0x44 40
0x45 Rx/Tx 3B_0x45 08
0x46 Rx/Tx 3B_0x46 02
0x47 Rx/Tx 3B_0x47 80
0x48 Rx/Tx 3B_0x48 03
0x49 Rx/Tx 3B_0x49 0C
0x4A Rx/Tx 3B_0x4A 30
0x4B Rx/Tx 3B_0x4B 41
0x4C Rx/Tx 3B_0x4C 50
0x4D Rx/Tx 3B_0x4D C0
0x4E Rx/Tx 3B_0x4E 60
0x4F Rx/Tx 3B_0x4F 90
0x50 Rx/Tx 3B_0x50 88
0x51 Rx/Tx 3B_0x51 82
0x52 Rx/Tx 3B_0x52 A0
0x53 Rx/Tx 3B_0x53 46
0x54 Rx/Tx 3B_0x54 52
0x55 Rx/Tx 3B_0x55 8C
0x56 Rx/Tx 3B_0x56 B0
0x57 Rx/Tx 3B_0x57 C8
0x58 Rx/Tx 3B_0x58 57
0x59 Rx/Tx 3B_0x59 5D
0x5A Rx/Tx 3B_0x5A 69
0x5B Rx/Tx 3B_0x5B 75
0x5C Rx/Tx 3B_0x5C D5
0x5D Rx/Tx 3B_0x5D 99
0x5E Rx/Tx 3B_0x5E 96
0x5F Rx/Tx 3B_0x5F A5
0x60 Rx/Tx 3B_0x60 00
0x61 Rx/Tx 3B_0x61 00
0x62 Rx/Tx 3B_0x62 00
0x63 Rx/Tx 3B_0x63 00
0x64 Rx/Tx 3B_0x64 00
0x65 Rx/Tx 3B_0x65 00
0x66 Rx/Tx 3B_0x66 00
0x67 Rx/Tx 3B_0x67 20
0x68 Rx/Tx 3B_0x68 00
0x69 Rx/Tx 3B_0x69 0A
0x6A Rx/Tx 3B_0x6A 22
0x6B Rx/Tx 3B_0x6B 40
0x6C Rx/Tx 3B_0x6C 00
0x6D Rx/Tx 3B_0x6D 00
0x6E Rx/Tx 3B_0x6E 00
0x6F Rx/Tx 3B_0x6F 00
0x70 Rx/Tx 3B_0x70 03
0x71 Rx/Tx 3B_0x71 20
0x72 Rx/Tx 3B_0x72 00
0x73 Rx/Tx 3B_0x73 00
0x74 Rx/Tx 3B_0x74 00
0x75 Rx/Tx 3B_0x75 00
0x76 Rx/Tx 3B_0x76 22
0x77 Rx/Tx 3B_0x77 1A
0x78 Rx/Tx 3B_0x78 30
0x79 Rx/Tx 3B_0x79 10
0x7A Rx/Tx 3B_0x7A 00
0x7B Rx/Tx 3B_0x7B 00
0x7C Rx/Tx 3B_0x7C 00
0x7D Rx/Tx 3B_0x7D 48
0x7E Rx/Tx 3B_0x7E 13
0x7F Rx/Tx 3B_0x7F 3A
0x80 Rx/Tx 3B_0x80 04
0x81 Rx/Tx 3B_0x81 E4
0x82 Rx/Tx 3B_0x82 00
0x83 Rx/Tx 3B_0x83 07
0x84 Rx/Tx 3B_0x84 FF
0x85 Rx/Tx 3B_0x85 00
0x86 Rx/Tx 3B_0x86 00
0x87 Rx/Tx 3B_0x87 00
0x88 Rx/Tx 3B_0x88 00
0x89 Rx/Tx 3B_0x89 00
0x8A Rx/Tx 3B_0x8A 33
0x8B Rx/Tx 3B_0x8B 00
0x8C Rx/Tx 3B_0x8C 00
0x8D Rx/Tx 3B_0x8D 02
0x8E Rx/Tx 3B_0x8E 1C
0x8F Rx/Tx 3B_0x8F 00
0x90 Rx/Tx 3B_0x90 00
0x91 Rx/Tx 3B_0x91 00
0x92 Rx/Tx 3B_0x92 00
0x93 Rx/Tx 3B_0x93 00
0x94 Rx/Tx 3B_0x94 00
0x95 Rx/Tx 3B_0x95 00
0x96 Rx/Tx 3B_0x96 04
0x97 Rx/Tx 3B_0x97 00
0x98 Rx/Tx 3B_0x98 0C
0x99 Rx/Tx 3B_0x99 3F
0x9A Rx/Tx 3B_0x9A 3F
0x9B Rx/Tx 3B_0x9B 00
0x0 Rx/Tx 4A_0x00 00
0x1 Rx/Tx 4A_0x01 00
0x2 Rx/Tx 4A_0x02 00
0x3 Rx/Tx 4A_0x03 00
0x4 Rx/Tx 4A_0x04 01
0x5 Rx/Tx 4A_0x05 01
0x6 Rx/Tx 4A_0x06 01
0x7 Rx/Tx 4A_0x07 01
0x8 Rx/Tx 4A_0x08 60
0x9 Rx/Tx 4A_0x09 00
0xA Rx/Tx 4A_0x0A 50
0xB Rx/Tx 4A_0x0B 6F
0xC Rx/Tx 4A_0x0C 08
0xD Rx/Tx 4A_0x0D B4
0xE Rx/Tx 4A_0x0E 93
0xF Rx/Tx 4A_0x0F 69
0x10 Rx/Tx 4A_0x10 3A
0x11 Rx/Tx 4A_0x11 20
0x12 Rx/Tx 4A_0x12 E0
0x13 Rx/Tx 4A_0x13 90
0x14 Rx/Tx 4A_0x14 00
0x15 Rx/Tx 4A_0x15 12
0x16 Rx/Tx 4A_0x16 7A
0x17 Rx/Tx 4A_0x17 36
0x18 Rx/Tx 4A_0x18 40
0x19 Rx/Tx 4A_0x19 20
0x1A Rx/Tx 4A_0x1A A0
0x1B Rx/Tx 4A_0x1B 03
0x1C Rx/Tx 4A_0x1C 90
0x1D Rx/Tx 4A_0x1D 00
0x1E Rx/Tx 4A_0x1E E9
0x1F Rx/Tx 4A_0x1F 55
0x20 Rx/Tx 4A_0x20 00
0x21 Rx/Tx 4A_0x21 00
0x22 Rx/Tx 4A_0x22 00
0x23 Rx/Tx 4A_0x23 40
0x24 Rx/Tx 4A_0x24 40
0x25 Rx/Tx 4A_0x25 00
0x26 Rx/Tx 4A_0x26 00
0x27 Rx/Tx 4A_0x27 00
0x28 Rx/Tx 4A_0x28 00
0x29 Rx/Tx 4A_0x29 00
0x2A Rx/Tx 4A_0x2A 30
0x2B Rx/Tx 4A_0x2B 0F
0x2C Rx/Tx 4A_0x2C F2
0x2D Rx/Tx 4A_0x2D 04
0x2E Rx/Tx 4A_0x2E 00
0x2F Rx/Tx 4A_0x2F 36
0x30 Rx/Tx 4A_0x30 00
0x31 Rx/Tx 4A_0x31 20
0x32 Rx/Tx 4A_0x32 11
0x33 Rx/Tx 4A_0x33 88
0x34 Rx/Tx 4A_0x34 BF
0x35 Rx/Tx 4A_0x35 1F
0x36 Rx/Tx 4A_0x36 30
0x37 Rx/Tx 4A_0x37 00
0x38 Rx/Tx 4A_0x38 00
0x39 Rx/Tx 4A_0x39 00
0x3A Rx/Tx 4A_0x3A 00
0x3B Rx/Tx 4A_0x3B 43
0x3C Rx/Tx 4A_0x3C 02
0x3D Rx/Tx 4A_0x3D 35
0x3E Rx/Tx 4A_0x3E 43
0x3F Rx/Tx 4A_0x3F C7
0x40 Rx/Tx 4A_0x40 00
0x41 Rx/Tx 4A_0x41 01
0x42 Rx/Tx 4A_0x42 04
0x43 Rx/Tx 4A_0x43 10
0x44 Rx/Tx 4A_0x44 40
0x45 Rx/Tx 4A_0x45 08
0x46 Rx/Tx 4A_0x46 02
0x47 Rx/Tx 4A_0x47 80
0x48 Rx/Tx 4A_0x48 03
0x49 Rx/Tx 4A_0x49 0C
0x4A Rx/Tx 4A_0x4A 30
0x4B Rx/Tx 4A_0x4B 41
0x4C Rx/Tx 4A_0x4C 50
0x4D Rx/Tx 4A_0x4D C0
0x4E Rx/Tx 4A_0x4E 60
0x4F Rx/Tx 4A_0x4F 90
0x50 Rx/Tx 4A_0x50 88
0x51 Rx/Tx 4A_0x51 82
0x52 Rx/Tx 4A_0x52 A0
0x53 Rx/Tx 4A_0x53 46
0x54 Rx/Tx 4A_0x54 52
0x55 Rx/Tx 4A_0x55 8C
0x56 Rx/Tx 4A_0x56 B0
0x57 Rx/Tx 4A_0x57 C8
0x58 Rx/Tx 4A_0x58 57
0x59 Rx/Tx 4A_0x59 5D
0x5A Rx/Tx 4A_0x5A 69
0x5B Rx/Tx 4A_0x5B 75
0x5C Rx/Tx 4A_0x5C D5
0x5D Rx/Tx 4A_0x5D 99
0x5E Rx/Tx 4A_0x5E 96
0x5F Rx/Tx 4A_0x5F A5
0x60 Rx/Tx 4A_0x60 00
0x61 Rx/Tx 4A_0x61 00
0x62 Rx/Tx 4A_0x62 00
0x63 Rx/Tx 4A_0x63 00
0x64 Rx/Tx 4A_0x64 00
0x65 Rx/Tx 4A_0x65 00
0x66 Rx/Tx 4A_0x66 00
0x67 Rx/Tx 4A_0x67 20
0x68 Rx/Tx 4A_0x68 00
0x69 Rx/Tx 4A_0x69 0A
0x6A Rx/Tx 4A_0x6A 22
0x6B Rx/Tx 4A_0x6B 40
0x6C Rx/Tx 4A_0x6C 00
0x6D Rx/Tx 4A_0x6D 00
0x6E Rx/Tx 4A_0x6E 00
0x6F Rx/Tx 4A_0x6F 00
0x70 Rx/Tx 4A_0x70 03
0x71 Rx/Tx 4A_0x71 20
0x72 Rx/Tx 4A_0x72 00
0x73 Rx/Tx 4A_0x73 00
0x74 Rx/Tx 4A_0x74 00
0x75 Rx/Tx 4A_0x75 00
0x76 Rx/Tx 4A_0x76 22
0x77 Rx/Tx 4A_0x77 1A
0x78 Rx/Tx 4A_0x78 00
0x79 Rx/Tx 4A_0x79 10
0x7A Rx/Tx 4A_0x7A 00
0x7B Rx/Tx 4A_0x7B 00
0x7C Rx/Tx 4A_0x7C 00
0x7D Rx/Tx 4A_0x7D 48
0x7E Rx/Tx 4A_0x7E 13
0x7F Rx/Tx 4A_0x7F 3A
0x80 Rx/Tx 4A_0x80 00
0x81 Rx/Tx 4A_0x81 E4
0x82 Rx/Tx 4A_0x82 00
0x83 Rx/Tx 4A_0x83 00
0x84 Rx/Tx 4A_0x84 00
0x85 Rx/Tx 4A_0x85 00
0x86 Rx/Tx 4A_0x86 00
0x87 Rx/Tx 4A_0x87 00
0x88 Rx/Tx 4A_0x88 00
0x89 Rx/Tx 4A_0x89 02
0x8A Rx/Tx 4A_0x8A DC
0x8B Rx/Tx 4A_0x8B 00
0x8C Rx/Tx 4A_0x8C 00
0x8D Rx/Tx 4A_0x8D 02
0x8E Rx/Tx 4A_0x8E 1C
0x8F Rx/Tx 4A_0x8F 00
0x90 Rx/Tx 4A_0x90 00
0x91 Rx/Tx 4A_0x91 00
0x92 Rx/Tx 4A_0x92 00
0x93 Rx/Tx 4A_0x93 00
0x94 Rx/Tx 4A_0x94 00
0x95 Rx/Tx 4A_0x95 00
0x96 Rx/Tx 4A_0x96 04
0x97 Rx/Tx 4A_0x97 00
0x98 Rx/Tx 4A_0x98 0C
0x99 Rx/Tx 4A_0x99 3F
0x9A Rx/Tx 4A_0x9A 3F
0x9B Rx/Tx 4A_0x9B 00
0x0 Rx/Tx 4B_0x00 00
0x1 Rx/Tx 4B_0x01 00
0x2 Rx/Tx 4B_0x02 00
0x3 Rx/Tx 4B_0x03 00
0x4 Rx/Tx 4B_0x04 01
0x5 Rx/Tx 4B_0x05 01
0x6 Rx/Tx 4B_0x06 01
0x7 Rx/Tx 4B_0x07 01
0x8 Rx/Tx 4B_0x08 60
0x9 Rx/Tx 4B_0x09 00
0xA Rx/Tx 4B_0x0A 50
0xB Rx/Tx 4B_0x0B 6F
0xC Rx/Tx 4B_0x0C 08
0xD Rx/Tx 4B_0x0D B4
0xE Rx/Tx 4B_0x0E 93
0xF Rx/Tx 4B_0x0F 69
0x10 Rx/Tx 4B_0x10 3A
0x11 Rx/Tx 4B_0x11 20
0x12 Rx/Tx 4B_0x12 E0
0x13 Rx/Tx 4B_0x13 90
0x14 Rx/Tx 4B_0x14 00
0x15 Rx/Tx 4B_0x15 12
0x16 Rx/Tx 4B_0x16 7A
0x17 Rx/Tx 4B_0x17 36
0x18 Rx/Tx 4B_0x18 40
0x19 Rx/Tx 4B_0x19 20
0x1A Rx/Tx 4B_0x1A A0
0x1B Rx/Tx 4B_0x1B 03
0x1C Rx/Tx 4B_0x1C 90
0x1D Rx/Tx 4B_0x1D 00
0x1E Rx/Tx 4B_0x1E E9
0x1F Rx/Tx 4B_0x1F 55
0x20 Rx/Tx 4B_0x20 00
0x21 Rx/Tx 4B_0x21 00
0x22 Rx/Tx 4B_0x22 00
0x23 Rx/Tx 4B_0x23 40
0x24 Rx/Tx 4B_0x24 40
0x25 Rx/Tx 4B_0x25 00
0x26 Rx/Tx 4B_0x26 00
0x27 Rx/Tx 4B_0x27 00
0x28 Rx/Tx 4B_0x28 00
0x29 Rx/Tx 4B_0x29 00
0x2A Rx/Tx 4B_0x2A 30
0x2B Rx/Tx 4B_0x2B 0F
0x2C Rx/Tx 4B_0x2C F2
0x2D Rx/Tx 4B_0x2D 04
0x2E Rx/Tx 4B_0x2E 00
0x2F Rx/Tx 4B_0x2F 36
0x30 Rx/Tx 4B_0x30 00
0x31 Rx/Tx 4B_0x31 20
0x32 Rx/Tx 4B_0x32 11
0x33 Rx/Tx 4B_0x33 88
0x34 Rx/Tx 4B_0x34 BF
0x35 Rx/Tx 4B_0x35 1F
0x36 Rx/Tx 4B_0x36 30
0x37 Rx/Tx 4B_0x37 00
0x38 Rx/Tx 4B_0x38 00
0x39 Rx/Tx 4B_0x39 00
0x3A Rx/Tx 4B_0x3A 00
0x3B Rx/Tx 4B_0x3B 43
0x3C Rx/Tx 4B_0x3C 00
0x3D Rx/Tx 4B_0x3D 35
0x3E Rx/Tx 4B_0x3E 43
0x3F Rx/Tx 4B_0x3F C7
0x40 Rx/Tx 4B_0x40 00
0x41 Rx/Tx 4B_0x41 01
0x42 Rx/Tx 4B_0x42 04
0x43 Rx/Tx 4B_0x43 10
0x44 Rx/Tx 4B_0x44 40
0x45 Rx/Tx 4B_0x45 08
0x46 Rx/Tx 4B_0x46 02
0x47 Rx/Tx 4B_0x47 80
0x48 Rx/Tx 4B_0x48 03
0x49 Rx/Tx 4B_0x49 0C
0x4A Rx/Tx 4B_0x4A 30
0x4B Rx/Tx 4B_0x4B 41
0x4C Rx/Tx 4B_0x4C 50
0x4D Rx/Tx 4B_0x4D C0
0x4E Rx/Tx 4B_0x4E 60
0x4F Rx/Tx 4B_0x4F 90
0x50 Rx/Tx 4B_0x50 88
0x51 Rx/Tx 4B_0x51 82
0x52 Rx/Tx 4B_0x52 A0
0x53 Rx/Tx 4B_0x53 46
0x54 Rx/Tx 4B_0x54 52
0x55 Rx/Tx 4B_0x55 8C
0x56 Rx/Tx 4B_0x56 B0
0x57 Rx/Tx 4B_0x57 C8
0x58 Rx/Tx 4B_0x58 57
0x59 Rx/Tx 4B_0x59 5D
0x5A Rx/Tx 4B_0x5A 69
0x5B Rx/Tx 4B_0x5B 75
0x5C Rx/Tx 4B_0x5C D5
0x5D Rx/Tx 4B_0x5D 99
0x5E Rx/Tx 4B_0x5E 96
0x5F Rx/Tx 4B_0x5F A5
0x60 Rx/Tx 4B_0x60 00
0x61 Rx/Tx 4B_0x61 00
0x62 Rx/Tx 4B_0x62 00
0x63 Rx/Tx 4B_0x63 00
0x64 Rx/Tx 4B_0x64 00
0x65 Rx/Tx 4B_0x65 00
0x66 Rx/Tx 4B_0x66 00
0x67 Rx/Tx 4B_0x67 20
0x68 Rx/Tx 4B_0x68 00
0x69 Rx/Tx 4B_0x69 0A
0x6A Rx/Tx 4B_0x6A 22
0x6B Rx/Tx 4B_0x6B 40
0x6C Rx/Tx 4B_0x6C 00
0x6D Rx/Tx 4B_0x6D 00
0x6E Rx/Tx 4B_0x6E 00
0x6F Rx/Tx 4B_0x6F 00
0x70 Rx/Tx 4B_0x70 03
0x71 Rx/Tx 4B_0x71 20
0x72 Rx/Tx 4B_0x72 00
0x73 Rx/Tx 4B_0x73 00
0x74 Rx/Tx 4B_0x74 00
0x75 Rx/Tx 4B_0x75 00
0x76 Rx/Tx 4B_0x76 22
0x77 Rx/Tx 4B_0x77 1A
0x78 Rx/Tx 4B_0x78 00
0x79 Rx/Tx 4B_0x79 10
0x7A Rx/Tx 4B_0x7A 00
0x7B Rx/Tx 4B_0x7B 00
0x7C Rx/Tx 4B_0x7C 00
0x7D Rx/Tx 4B_0x7D 48
0x7E Rx/Tx 4B_0x7E 13
0x7F Rx/Tx 4B_0x7F 3A
0x80 Rx/Tx 4B_0x80 00
0x81 Rx/Tx 4B_0x81 E4
0x82 Rx/Tx 4B_0x82 00
0x83 Rx/Tx 4B_0x83 00
0x84 Rx/Tx 4B_0x84 00
0x85 Rx/Tx 4B_0x85 08
0x86 Rx/Tx 4B_0x86 00
0x87 Rx/Tx 4B_0x87 00
0x88 Rx/Tx 4B_0x88 00
0x89 Rx/Tx 4B_0x89 00
0x8A Rx/Tx 4B_0x8A 00
0x8B Rx/Tx 4B_0x8B 00
0x8C Rx/Tx 4B_0x8C 00
0x8D Rx/Tx 4B_0x8D 02
0x8E Rx/Tx 4B_0x8E 1C
0x8F Rx/Tx 4B_0x8F 00
0x90 Rx/Tx 4B_0x90 00
0x91 Rx/Tx 4B_0x91 00
0x92 Rx/Tx 4B_0x92 00
0x93 Rx/Tx 4B_0x93 00
0x94 Rx/Tx 4B_0x94 00
0x95 Rx/Tx 4B_0x95 00
0x96 Rx/Tx 4B_0x96 04
0x97 Rx/Tx 4B_0x97 00
0x98 Rx/Tx 4B_0x98 0C
0x99 Rx/Tx 4B_0x99 3F
0x9A Rx/Tx 4B_0x9A 3F
0x9B Rx/Tx 4B_0x9B 00
0x0 Rx/Tx 5A_0x00 00
0x1 Rx/Tx 5A_0x01 00
0x2 Rx/Tx 5A_0x02 00
0x3 Rx/Tx 5A_0x03 00
0x4 Rx/Tx 5A_0x04 01
0x5 Rx/Tx 5A_0x05 01
0x6 Rx/Tx 5A_0x06 01
0x7 Rx/Tx 5A_0x07 01
0x8 Rx/Tx 5A_0x08 60
0x9 Rx/Tx 5A_0x09 00
0xA Rx/Tx 5A_0x0A 50
0xB Rx/Tx 5A_0x0B 6F
0xC Rx/Tx 5A_0x0C 08
0xD Rx/Tx 5A_0x0D B4
0xE Rx/Tx 5A_0x0E 93
0xF Rx/Tx 5A_0x0F 69
0x10 Rx/Tx 5A_0x10 3A
0x11 Rx/Tx 5A_0x11 20
0x12 Rx/Tx 5A_0x12 E0
0x13 Rx/Tx 5A_0x13 90
0x14 Rx/Tx 5A_0x14 00
0x15 Rx/Tx 5A_0x15 12
0x16 Rx/Tx 5A_0x16 7A
0x17 Rx/Tx 5A_0x17 36
0x18 Rx/Tx 5A_0x18 40
0x19 Rx/Tx 5A_0x19 20
0x1A Rx/Tx 5A_0x1A A0
0x1B Rx/Tx 5A_0x1B 03
0x1C Rx/Tx 5A_0x1C 90
0x1D Rx/Tx 5A_0x1D 00
0x1E Rx/Tx 5A_0x1E E9
0x1F Rx/Tx 5A_0x1F 55
0x20 Rx/Tx 5A_0x20 00
0x21 Rx/Tx 5A_0x21 00
0x22 Rx/Tx 5A_0x22 00
0x23 Rx/Tx 5A_0x23 40
0x24 Rx/Tx 5A_0x24 40
0x25 Rx/Tx 5A_0x25 00
0x26 Rx/Tx 5A_0x26 00
0x27 Rx/Tx 5A_0x27 00
0x28 Rx/Tx 5A_0x28 00
0x29 Rx/Tx 5A_0x29 00
0x2A Rx/Tx 5A_0x2A 30
0x2B Rx/Tx 5A_0x2B 0F
0x2C Rx/Tx 5A_0x2C F2
0x2D Rx/Tx 5A_0x2D 04
0x2E Rx/Tx 5A_0x2E 00
0x2F Rx/Tx 5A_0x2F 36
0x30 Rx/Tx 5A_0x30 00
0x31 Rx/Tx 5A_0x31 20
0x32 Rx/Tx 5A_0x32 11
0x33 Rx/Tx 5A_0x33 88
0x34 Rx/Tx 5A_0x34 BF
0x35 Rx/Tx 5A_0x35 1F
0x36 Rx/Tx 5A_0x36 30
0x37 Rx/Tx 5A_0x37 00
0x38 Rx/Tx 5A_0x38 00
0x39 Rx/Tx 5A_0x39 00
0x3A Rx/Tx 5A_0x3A 00
0x3B Rx/Tx 5A_0x3B 43
0x3C Rx/Tx 5A_0x3C 03
0x3D Rx/Tx 5A_0x3D 35
0x3E Rx/Tx 5A_0x3E 43
0x3F Rx/Tx 5A_0x3F C7
0x40 Rx/Tx 5A_0x40 00
0x41 Rx/Tx 5A_0x41 01
0x42 Rx/Tx 5A_0x42 04
0x43 Rx/Tx 5A_0x43 10
0x44 Rx/Tx 5A_0x44 40
0x45 Rx/Tx 5A_0x45 08
0x46 Rx/Tx 5A_0x46 02
0x47 Rx/Tx 5A_0x47 80
0x48 Rx/Tx 5A_0x48 03
0x49 Rx/Tx 5A_0x49 0C
0x4A Rx/Tx 5A_0x4A 30
0x4B Rx/Tx 5A_0x4B 41
0x4C Rx/Tx 5A_0x4C 50
0x4D Rx/Tx 5A_0x4D C0
0x4E Rx/Tx 5A_0x4E 60
0x4F Rx/Tx 5A_0x4F 90
0x50 Rx/Tx 5A_0x50 88
0x51 Rx/Tx 5A_0x51 82
0x52 Rx/Tx 5A_0x52 A0
0x53 Rx/Tx 5A_0x53 46
0x54 Rx/Tx 5A_0x54 52
0x55 Rx/Tx 5A_0x55 8C
0x56 Rx/Tx 5A_0x56 B0
0x57 Rx/Tx 5A_0x57 C8
0x58 Rx/Tx 5A_0x58 57
0x59 Rx/Tx 5A_0x59 5D
0x5A Rx/Tx 5A_0x5A 69
0x5B Rx/Tx 5A_0x5B 75
0x5C Rx/Tx 5A_0x5C D5
0x5D Rx/Tx 5A_0x5D 99
0x5E Rx/Tx 5A_0x5E 96
0x5F Rx/Tx 5A_0x5F A5
0x60 Rx/Tx 5A_0x60 00
0x61 Rx/Tx 5A_0x61 00
0x62 Rx/Tx 5A_0x62 00
0x63 Rx/Tx 5A_0x63 00
0x64 Rx/Tx 5A_0x64 00
0x65 Rx/Tx 5A_0x65 00
0x66 Rx/Tx 5A_0x66 00
0x67 Rx/Tx 5A_0x67 20
0x68 Rx/Tx 5A_0x68 00
0x69 Rx/Tx 5A_0x69 0A
0x6A Rx/Tx 5A_0x6A 22
0x6B Rx/Tx 5A_0x6B 40
0x6C Rx/Tx 5A_0x6C 00
0x6D Rx/Tx 5A_0x6D 00
0x6E Rx/Tx 5A_0x6E 00
0x6F Rx/Tx 5A_0x6F 00
0x70 Rx/Tx 5A_0x70 03
0x71 Rx/Tx 5A_0x71 20
0x72 Rx/Tx 5A_0x72 00
0x73 Rx/Tx 5A_0x73 00
0x74 Rx/Tx 5A_0x74 00
0x75 Rx/Tx 5A_0x75 00
0x76 Rx/Tx 5A_0x76 22
0x77 Rx/Tx 5A_0x77 1A
0x78 Rx/Tx 5A_0x78 00
0x79 Rx/Tx 5A_0x79 10
0x7A Rx/Tx 5A_0x7A 00
0x7B Rx/Tx 5A_0x7B 00
0x7C Rx/Tx 5A_0x7C 00
0x7D Rx/Tx 5A_0x7D 48
0x7E Rx/Tx 5A_0x7E 13
0x7F Rx/Tx 5A_0x7F 3A
0x80 Rx/Tx 5A_0x80 00
0x81 Rx/Tx 5A_0x81 E4
0x82 Rx/Tx 5A_0x82 00
0x83 Rx/Tx 5A_0x83 00
0x84 Rx/Tx 5A_0x84 00
0x85 Rx/Tx 5A_0x85 00
0x86 Rx/Tx 5A_0x86 00
0x87 Rx/Tx 5A_0x87 00
0x88 Rx/Tx 5A_0x88 00
0x89 Rx/Tx 5A_0x89 02
0x8A Rx/Tx 5A_0x8A FF
0x8B Rx/Tx 5A_0x8B 00
0x8C Rx/Tx 5A_0x8C 00
0x8D Rx/Tx 5A_0x8D 02
0x8E Rx/Tx 5A_0x8E 1C
0x8F Rx/Tx 5A_0x8F 00
0x90 Rx/Tx 5A_0x90 00
0x91 Rx/Tx 5A_0x91 00
0x92 Rx/Tx 5A_0x92 00
0x93 Rx/Tx 5A_0x93 00
0x94 Rx/Tx 5A_0x94 00
0x95 Rx/Tx 5A_0x95 00
0x96 Rx/Tx 5A_0x96 04
0x97 Rx/Tx 5A_0x97 00
0x98 Rx/Tx 5A_0x98 0C
0x99 Rx/Tx 5A_0x99 3F
0x9A Rx/Tx 5A_0x9A 3F
0x9B Rx/Tx 5A_0x9B 00
0x0 Rx/Tx 5B_0x00 00
0x1 Rx/Tx 5B_0x01 00
0x2 Rx/Tx 5B_0x02 00
0x3 Rx/Tx 5B_0x03 00
0x4 Rx/Tx 5B_0x04 01
0x5 Rx/Tx 5B_0x05 01
0x6 Rx/Tx 5B_0x06 01
0x7 Rx/Tx 5B_0x07 01
0x8 Rx/Tx 5B_0x08 60
0x9 Rx/Tx 5B_0x09 00
0xA Rx/Tx 5B_0x0A 50
0xB Rx/Tx 5B_0x0B 6F
0xC Rx/Tx 5B_0x0C 08
0xD Rx/Tx 5B_0x0D B4
0xE Rx/Tx 5B_0x0E 93
0xF Rx/Tx 5B_0x0F 69
0x10 Rx/Tx 5B_0x10 3A
0x11 Rx/Tx 5B_0x11 20
0x12 Rx/Tx 5B_0x12 E0
0x13 Rx/Tx 5B_0x13 90
0x14 Rx/Tx 5B_0x14 00
0x15 Rx/Tx 5B_0x15 12
0x16 Rx/Tx 5B_0x16 7A
0x17 Rx/Tx 5B_0x17 36
0x18 Rx/Tx 5B_0x18 40
0x19 Rx/Tx 5B_0x19 20
0x1A Rx/Tx 5B_0x1A A0
0x1B Rx/Tx 5B_0x1B 03
0x1C Rx/Tx 5B_0x1C 90
0x1D Rx/Tx 5B_0x1D 00
0x1E Rx/Tx 5B_0x1E E9
0x1F Rx/Tx 5B_0x1F 55
0x20 Rx/Tx 5B_0x20 00
0x21 Rx/Tx 5B_0x21 00
0x22 Rx/Tx 5B_0x22 00
0x23 Rx/Tx 5B_0x23 40
0x24 Rx/Tx 5B_0x24 40
0x25 Rx/Tx 5B_0x25 00
0x26 Rx/Tx 5B_0x26 00
0x27 Rx/Tx 5B_0x27 00
0x28 Rx/Tx 5B_0x28 00
0x29 Rx/Tx 5B_0x29 00
0x2A Rx/Tx 5B_0x2A 30
0x2B Rx/Tx 5B_0x2B 0F
0x2C Rx/Tx 5B_0x2C F2
0x2D Rx/Tx 5B_0x2D 04
0x2E Rx/Tx 5B_0x2E 00
0x2F Rx/Tx 5B_0x2F 36
0x30 Rx/Tx 5B_0x30 00
0x31 Rx/Tx 5B_0x31 20
0x32 Rx/Tx 5B_0x32 11
0x33 Rx/Tx 5B_0x33 88
0x34 Rx/Tx 5B_0x34 BF
0x35 Rx/Tx 5B_0x35 1F
0x36 Rx/Tx 5B_0x36 30
0x37 Rx/Tx 5B_0x37 00
0x38 Rx/Tx 5B_0x38 00
0x39 Rx/Tx 5B_0x39 00
0x3A Rx/Tx 5B_0x3A 00
0x3B Rx/Tx 5B_0x3B 42
0x3C Rx/Tx 5B_0x3C FD
0x3D Rx/Tx 5B_0x3D 35
0x3E Rx/Tx 5B_0x3E 43
0x3F Rx/Tx 5B_0x3F C7
0x40 Rx/Tx 5B_0x40 00
0x41 Rx/Tx 5B_0x41 01
0x42 Rx/Tx 5B_0x42 04
0x43 Rx/Tx 5B_0x43 10
0x44 Rx/Tx 5B_0x44 40
0x45 Rx/Tx 5B_0x45 08
0x46 Rx/Tx 5B_0x46 02
0x47 Rx/Tx 5B_0x47 80
0x48 Rx/Tx 5B_0x48 03
0x49 Rx/Tx 5B_0x49 0C
0x4A Rx/Tx 5B_0x4A 30
0x4B Rx/Tx 5B_0x4B 41
0x4C Rx/Tx 5B_0x4C 50
0x4D Rx/Tx 5B_0x4D C0
0x4E Rx/Tx 5B_0x4E 60
0x4F Rx/Tx 5B_0x4F 90
0x50 Rx/Tx 5B_0x50 88
0x51 Rx/Tx 5B_0x51 82
0x52 Rx/Tx 5B_0x52 A0
0x53 Rx/Tx 5B_0x53 46
0x54 Rx/Tx 5B_0x54 52
0x55 Rx/Tx 5B_0x55 8C
0x56 Rx/Tx 5B_0x56 B0
0x57 Rx/Tx 5B_0x57 C8
0x58 Rx/Tx 5B_0x58 57
0x59 Rx/Tx 5B_0x59 5D
0x5A Rx/Tx 5B_0x5A 69
0x5B Rx/Tx 5B_0x5B 75
0x5C Rx/Tx 5B_0x5C D5
0x5D Rx/Tx 5B_0x5D 99
0x5E Rx/Tx 5B_0x5E 96
0x5F Rx/Tx 5B_0x5F A5
0x60 Rx/Tx 5B_0x60 00
0x61 Rx/Tx 5B_0x61 00
0x62 Rx/Tx 5B_0x62 00
0x63 Rx/Tx 5B_0x63 00
0x64 Rx/Tx 5B_0x64 00
0x65 Rx/Tx 5B_0x65 00
0x66 Rx/Tx 5B_0x66 00
0x67 Rx/Tx 5B_0x67 20
0x68 Rx/Tx 5B_0x68 00
0x69 Rx/Tx 5B_0x69 0A
0x6A Rx/Tx 5B_0x6A 22
0x6B Rx/Tx 5B_0x6B 40
0x6C Rx/Tx 5B_0x6C 00
0x6D Rx/Tx 5B_0x6D 00
0x6E Rx/Tx 5B_0x6E 00
0x6F Rx/Tx 5B_0x6F 00
0x70 Rx/Tx 5B_0x70 03
0x71 Rx/Tx 5B_0x71 20
0x72 Rx/Tx 5B_0x72 00
0x73 Rx/Tx 5B_0x73 00
0x74 Rx/Tx 5B_0x74 00
0x75 Rx/Tx 5B_0x75 00
0x76 Rx/Tx 5B_0x76 22
0x77 Rx/Tx 5B_0x77 1A
0x78 Rx/Tx 5B_0x78 00
0x79 Rx/Tx 5B_0x79 10
0x7A Rx/Tx 5B_0x7A 00
0x7B Rx/Tx 5B_0x7B 00
0x7C Rx/Tx 5B_0x7C 00
0x7D Rx/Tx 5B_0x7D 48
0x7E Rx/Tx 5B_0x7E 13
0x7F Rx/Tx 5B_0x7F 3A
0x80 Rx/Tx 5B_0x80 00
0x81 Rx/Tx 5B_0x81 E4
0x82 Rx/Tx 5B_0x82 00
0x83 Rx/Tx 5B_0x83 00
0x84 Rx/Tx 5B_0x84 00
0x85 Rx/Tx 5B_0x85 00
0x86 Rx/Tx 5B_0x86 00
0x87 Rx/Tx 5B_0x87 00
0x88 Rx/Tx 5B_0x88 00
0x89 Rx/Tx 5B_0x89 00
0x8A Rx/Tx 5B_0x8A 13
0x8B Rx/Tx 5B_0x8B 00
0x8C Rx/Tx 5B_0x8C 00
0x8D Rx/Tx 5B_0x8D 02
0x8E Rx/Tx 5B_0x8E 1C
0x8F Rx/Tx 5B_0x8F 00
0x90 Rx/Tx 5B_0x90 00
0x91 Rx/Tx 5B_0x91 00
0x92 Rx/Tx 5B_0x92 00
0x93 Rx/Tx 5B_0x93 00
0x94 Rx/Tx 5B_0x94 00
0x95 Rx/Tx 5B_0x95 00
0x96 Rx/Tx 5B_0x96 04
0x97 Rx/Tx 5B_0x97 00
0x98 Rx/Tx 5B_0x98 0C
0x99 Rx/Tx 5B_0x99 3F
0x9A Rx/Tx 5B_0x9A 3F
0x9B Rx/Tx 5B_0x9B 00
0x0 Rx/Tx 6A_0x00 00
0x1 Rx/Tx 6A_0x01 00
0x2 Rx/Tx 6A_0x02 00
0x3 Rx/Tx 6A_0x03 00
0x4 Rx/Tx 6A_0x04 01
0x5 Rx/Tx 6A_0x05 01
0x6 Rx/Tx 6A_0x06 01
0x7 Rx/Tx 6A_0x07 01
0x8 Rx/Tx 6A_0x08 60
0x9 Rx/Tx 6A_0x09 00
0xA Rx/Tx 6A_0x0A 50
0xB Rx/Tx 6A_0x0B 6F
0xC Rx/Tx 6A_0x0C 08
0xD Rx/Tx 6A_0x0D B4
0xE Rx/Tx 6A_0x0E 93
0xF Rx/Tx 6A_0x0F 69
0x10 Rx/Tx 6A_0x10 3A
0x11 Rx/Tx 6A_0x11 20
0x12 Rx/Tx 6A_0x12 E0
0x13 Rx/Tx 6A_0x13 90
0x14 Rx/Tx 6A_0x14 00
0x15 Rx/Tx 6A_0x15 12
0x16 Rx/Tx 6A_0x16 7A
0x17 Rx/Tx 6A_0x17 36
0x18 Rx/Tx 6A_0x18 40
0x19 Rx/Tx 6A_0x19 20
0x1A Rx/Tx 6A_0x1A A0
0x1B Rx/Tx 6A_0x1B 03
0x1C Rx/Tx 6A_0x1C 90
0x1D Rx/Tx 6A_0x1D 00
0x1E Rx/Tx 6A_0x1E E9
0x1F Rx/Tx 6A_0x1F 55
0x20 Rx/Tx 6A_0x20 00
0x21 Rx/Tx 6A_0x21 00
0x22 Rx/Tx 6A_0x22 00
0x23 Rx/Tx 6A_0x23 40
0x24 Rx/Tx 6A_0x24 40
0x25 Rx/Tx 6A_0x25 00
0x26 Rx/Tx 6A_0x26 00
0x27 Rx/Tx 6A_0x27 00
0x28 Rx/Tx 6A_0x28 00
0x29 Rx/Tx 6A_0x29 01
0x2A Rx/Tx 6A_0x2A 30
0x2B Rx/Tx 6A_0x2B 0F
0x2C Rx/Tx 6A_0x2C F2
0x2D Rx/Tx 6A_0x2D 04
0x2E Rx/Tx 6A_0x2E 00
0x2F Rx/Tx 6A_0x2F 36
0x30 Rx/Tx 6A_0x30 00
0x31 Rx/Tx 6A_0x31 20
0x32 Rx/Tx 6A_0x32 11
0x33 Rx/Tx 6A_0x33 88
0x34 Rx/Tx 6A_0x34 BF
0x35 Rx/Tx 6A_0x35 1F
0x36 Rx/Tx 6A_0x36 30
0x37 Rx/Tx 6A_0x37 00
0x38 Rx/Tx 6A_0x38 00
0x39 Rx/Tx 6A_0x39 00
0x3A Rx/Tx 6A_0x3A 00
0x3B Rx/Tx 6A_0x3B 42
0x3C Rx/Tx 6A_0x3C FD
0x3D Rx/Tx 6A_0x3D 35
0x3E Rx/Tx 6A_0x3E 43
0x3F Rx/Tx 6A_0x3F C7
0x40 Rx/Tx 6A_0x40 00
0x41 Rx/Tx 6A_0x41 01
0x42 Rx/Tx 6A_0x42 04
0x43 Rx/Tx 6A_0x43 10
0x44 Rx/Tx 6A_0x44 40
0x45 Rx/Tx 6A_0x45 08
0x46 Rx/Tx 6A_0x46 02
0x47 Rx/Tx 6A_0x47 80
0x48 Rx/Tx 6A_0x48 03
0x49 Rx/Tx 6A_0x49 0C
0x4A Rx/Tx 6A_0x4A 30
0x4B Rx/Tx 6A_0x4B 41
0x4C Rx/Tx 6A_0x4C 50
0x4D Rx/Tx 6A_0x4D C0
0x4E Rx/Tx 6A_0x4E 60
0x4F Rx/Tx 6A_0x4F 90
0x50 Rx/Tx 6A_0x50 88
0x51 Rx/Tx 6A_0x51 82
0x52 Rx/Tx 6A_0x52 A0
0x53 Rx/Tx 6A_0x53 46
0x54 Rx/Tx 6A_0x54 52
0x55 Rx/Tx 6A_0x55 8C
0x56 Rx/Tx 6A_0x56 B0
0x57 Rx/Tx 6A_0x57 C8
0x58 Rx/Tx 6A_0x58 57
0x59 Rx/Tx 6A_0x59 5D
0x5A Rx/Tx 6A_0x5A 69
0x5B Rx/Tx 6A_0x5B 75
0x5C Rx/Tx 6A_0x5C D5
0x5D Rx/Tx 6A_0x5D 99
0x5E Rx/Tx 6A_0x5E 96
0x5F Rx/Tx 6A_0x5F A5
0x60 Rx/Tx 6A_0x60 00
0x61 Rx/Tx 6A_0x61 00
0x62 Rx/Tx 6A_0x62 00
0x63 Rx/Tx 6A_0x63 00
0x64 Rx/Tx 6A_0x64 00
0x65 Rx/Tx 6A_0x65 00
0x66 Rx/Tx 6A_0x66 00
0x67 Rx/Tx 6A_0x67 20
0x68 Rx/Tx 6A_0x68 00
0x69 Rx/Tx 6A_0x69 0A
0x6A Rx/Tx 6A_0x6A 22
0x6B Rx/Tx 6A_0x6B 40
0x6C Rx/Tx 6A_0x6C 00
0x6D Rx/Tx 6A_0x6D 00
0x6E Rx/Tx 6A_0x6E 00
0x6F Rx/Tx 6A_0x6F 00
0x70 Rx/Tx 6A_0x70 03
0x71 Rx/Tx 6A_0x71 20
0x72 Rx/Tx 6A_0x72 00
0x73 Rx/Tx 6A_0x73 00
0x74 Rx/Tx 6A_0x74 00
0x75 Rx/Tx 6A_0x75 00
0x76 Rx/Tx 6A_0x76 22
0x77 Rx/Tx 6A_0x77 1A
0x78 Rx/Tx 6A_0x78 00
0x79 Rx/Tx 6A_0x79 10
0x7A Rx/Tx 6A_0x7A 00
0x7B Rx/Tx 6A_0x7B 00
0x7C Rx/Tx 6A_0x7C 00
0x7D Rx/Tx 6A_0x7D 48
0x7E Rx/Tx 6A_0x7E 13
0x7F Rx/Tx 6A_0x7F 3A
0x80 Rx/Tx 6A_0x80 00
0x81 Rx/Tx 6A_0x81 E4
0x82 Rx/Tx 6A_0x82 00
0x83 Rx/Tx 6A_0x83 00
0x84 Rx/Tx 6A_0x84 00
0x85 Rx/Tx 6A_0x85 00
0x86 Rx/Tx 6A_0x86 00
0x87 Rx/Tx 6A_0x87 00
0x88 Rx/Tx 6A_0x88 00
0x89 Rx/Tx 6A_0x89 00
0x8A Rx/Tx 6A_0x8A 00
0x8B Rx/Tx 6A_0x8B 00
0x8C Rx/Tx 6A_0x8C 00
0x8D Rx/Tx 6A_0x8D 02
0x8E Rx/Tx 6A_0x8E 1C
0x8F Rx/Tx 6A_0x8F 00
0x90 Rx/Tx 6A_0x90 00
0x91 Rx/Tx 6A_0x91 00
0x92 Rx/Tx 6A_0x92 00
0x93 Rx/Tx 6A_0x93 00
0x94 Rx/Tx 6A_0x94 00
0x95 Rx/Tx 6A_0x95 00
0x96 Rx/Tx 6A_0x96 04
0x97 Rx/Tx 6A_0x97 00
0x98 Rx/Tx 6A_0x98 0C
0x99 Rx/Tx 6A_0x99 3F
0x9A Rx/Tx 6A_0x9A 3F
0x9B Rx/Tx 6A_0x9B 00
0x0 Rx/Tx 6B_0x00 00
0x1 Rx/Tx 6B_0x01 00
0x2 Rx/Tx 6B_0x02 00
0x3 Rx/Tx 6B_0x03 00
0x4 Rx/Tx 6B_0x04 01
0x5 Rx/Tx 6B_0x05 01
0x6 Rx/Tx 6B_0x06 01
0x7 Rx/Tx 6B_0x07 01
0x8 Rx/Tx 6B_0x08 60
0x9 Rx/Tx 6B_0x09 00
0xA Rx/Tx 6B_0x0A 50
0xB Rx/Tx 6B_0x0B 6F
0xC Rx/Tx 6B_0x0C 08
0xD Rx/Tx 6B_0x0D B4
0xE Rx/Tx 6B_0x0E 93
0xF Rx/Tx 6B_0x0F 69
0x10 Rx/Tx 6B_0x10 3A
0x11 Rx/Tx 6B_0x11 20
0x12 Rx/Tx 6B_0x12 E0
0x13 Rx/Tx 6B_0x13 90
0x14 Rx/Tx 6B_0x14 00
0x15 Rx/Tx 6B_0x15 12
0x16 Rx/Tx 6B_0x16 7A
0x17 Rx/Tx 6B_0x17 36
0x18 Rx/Tx 6B_0x18 40
0x19 Rx/Tx 6B_0x19 20
0x1A Rx/Tx 6B_0x1A A0
0x1B Rx/Tx 6B_0x1B 03
0x1C Rx/Tx 6B_0x1C 90
0x1D Rx/Tx 6B_0x1D 00
0x1E Rx/Tx 6B_0x1E E9
0x1F Rx/Tx 6B_0x1F 55
0x20 Rx/Tx 6B_0x20 00
0x21 Rx/Tx 6B_0x21 00
0x22 Rx/Tx 6B_0x22 00
0x23 Rx/Tx 6B_0x23 40
0x24 Rx/Tx 6B_0x24 40
0x25 Rx/Tx 6B_0x25 00
0x26 Rx/Tx 6B_0x26 00
0x27 Rx/Tx 6B_0x27 00
0x28 Rx/Tx 6B_0x28 00
0x29 Rx/Tx 6B_0x29 00
0x2A Rx/Tx 6B_0x2A 30
0x2B Rx/Tx 6B_0x2B 0F
0x2C Rx/Tx 6B_0x2C F2
0x2D Rx/Tx 6B_0x2D 04
0x2E Rx/Tx 6B_0x2E 00
0x2F Rx/Tx 6B_0x2F 36
0x30 Rx/Tx 6B_0x30 00
0x31 Rx/Tx 6B_0x31 20
0x32 Rx/Tx 6B_0x32 11
0x33 Rx/Tx 6B_0x33 88
0x34 Rx/Tx 6B_0x34 BF
0x35 Rx/Tx 6B_0x35 1F
0x36 Rx/Tx 6B_0x36 30
0x37 Rx/Tx 6B_0x37 00
0x38 Rx/Tx 6B_0x38 00
0x39 Rx/Tx 6B_0x39 00
0x3A Rx/Tx 6B_0x3A 00
0x3B Rx/Tx 6B_0x3B 42
0x3C Rx/Tx 6B_0x3C F3
0x3D Rx/Tx 6B_0x3D 35
0x3E Rx/Tx 6B_0x3E 43
0x3F Rx/Tx 6B_0x3F C7
0x40 Rx/Tx 6B_0x40 00
0x41 Rx/Tx 6B_0x41 01
0x42 Rx/Tx 6B_0x42 04
0x43 Rx/Tx 6B_0x43 10
0x44 Rx/Tx 6B_0x44 40
0x45 Rx/Tx 6B_0x45 08
0x46 Rx/Tx 6B_0x46 02
0x47 Rx/Tx 6B_0x47 80
0x48 Rx/Tx 6B_0x48 03
0x49 Rx/Tx 6B_0x49 0C
0x4A Rx/Tx 6B_0x4A 30
0x4B Rx/Tx 6B_0x4B 41
0x4C Rx/Tx 6B_0x4C 50
0x4D Rx/Tx 6B_0x4D C0
0x4E Rx/Tx 6B_0x4E 60
0x4F Rx/Tx 6B_0x4F 90
0x50 Rx/Tx 6B_0x50 88
0x51 Rx/Tx 6B_0x51 82
0x52 Rx/Tx 6B_0x52 A0
0x53 Rx/Tx 6B_0x53 46
0x54 Rx/Tx 6B_0x54 52
0x55 Rx/Tx 6B_0x55 8C
0x56 Rx/Tx 6B_0x56 B0
0x57 Rx/Tx 6B_0x57 C8
0x58 Rx/Tx 6B_0x58 57
0x59 Rx/Tx 6B_0x59 5D
0x5A Rx/Tx 6B_0x5A 69
0x5B Rx/Tx 6B_0x5B 75
0x5C Rx/Tx 6B_0x5C D5
0x5D Rx/Tx 6B_0x5D 99
0x5E Rx/Tx 6B_0x5E 96
0x5F Rx/Tx 6B_0x5F A5
0x60 Rx/Tx 6B_0x60 00
0x61 Rx/Tx 6B_0x61 00
0x62 Rx/Tx 6B_0x62 00
0x63 Rx/Tx 6B_0x63 00
0x64 Rx/Tx 6B_0x64 00
0x65 Rx/Tx 6B_0x65 00
0x66 Rx/Tx 6B_0x66 00
0x67 Rx/Tx 6B_0x67 20
0x68 Rx/Tx 6B_0x68 00
0x69 Rx/Tx 6B_0x69 0A
0x6A Rx/Tx 6B_0x6A 22
0x6B Rx/Tx 6B_0x6B 40
0x6C Rx/Tx 6B_0x6C 00
0x6D Rx/Tx 6B_0x6D 00
0x6E Rx/Tx 6B_0x6E 00
0x6F Rx/Tx 6B_0x6F 00
0x70 Rx/Tx 6B_0x70 03
0x71 Rx/Tx 6B_0x71 20
0x72 Rx/Tx 6B_0x72 00
0x73 Rx/Tx 6B_0x73 00
0x74 Rx/Tx 6B_0x74 00
0x75 Rx/Tx 6B_0x75 00
0x76 Rx/Tx 6B_0x76 22
0x77 Rx/Tx 6B_0x77 1A
0x78 Rx/Tx 6B_0x78 00
0x79 Rx/Tx 6B_0x79 10
0x7A Rx/Tx 6B_0x7A 00
0x7B Rx/Tx 6B_0x7B 00
0x7C Rx/Tx 6B_0x7C 00
0x7D Rx/Tx 6B_0x7D 48
0x7E Rx/Tx 6B_0x7E 13
0x7F Rx/Tx 6B_0x7F 3A
0x80 Rx/Tx 6B_0x80 00
0x81 Rx/Tx 6B_0x81 E4
0x82 Rx/Tx 6B_0x82 00
0x83 Rx/Tx 6B_0x83 00
0x84 Rx/Tx 6B_0x84 00
0x85 Rx/Tx 6B_0x85 00
0x86 Rx/Tx 6B_0x86 00
0x87 Rx/Tx 6B_0x87 00
0x88 Rx/Tx 6B_0x88 00
0x89 Rx/Tx 6B_0x89 02
0x8A Rx/Tx 6B_0x8A AD
0x8B Rx/Tx 6B_0x8B 00
0x8C Rx/Tx 6B_0x8C 00
0x8D Rx/Tx 6B_0x8D 02
0x8E Rx/Tx 6B_0x8E 1C
0x8F Rx/Tx 6B_0x8F 00
0x90 Rx/Tx 6B_0x90 00
0x91 Rx/Tx 6B_0x91 00
0x92 Rx/Tx 6B_0x92 00
0x93 Rx/Tx 6B_0x93 00
0x94 Rx/Tx 6B_0x94 00
0x95 Rx/Tx 6B_0x95 00
0x96 Rx/Tx 6B_0x96 04
0x97 Rx/Tx 6B_0x97 00
0x98 Rx/Tx 6B_0x98 0C
0x99 Rx/Tx 6B_0x99 3F
0x9A Rx/Tx 6B_0x9A 3F
0x9B Rx/Tx 6B_0x9B 00
0x0 Rx/Tx 7A_0x00 00
0x1 Rx/Tx 7A_0x01 00
0x2 Rx/Tx 7A_0x02 00
0x3 Rx/Tx 7A_0x03 00
0x4 Rx/Tx 7A_0x04 01
0x5 Rx/Tx 7A_0x05 01
0x6 Rx/Tx 7A_0x06 01
0x7 Rx/Tx 7A_0x07 01
0x8 Rx/Tx 7A_0x08 60
0x9 Rx/Tx 7A_0x09 00
0xA Rx/Tx 7A_0x0A 50
0xB Rx/Tx 7A_0x0B 6F
0xC Rx/Tx 7A_0x0C 08
0xD Rx/Tx 7A_0x0D B4
0xE Rx/Tx 7A_0x0E 93
0xF Rx/Tx 7A_0x0F 69
0x10 Rx/Tx 7A_0x10 3A
0x11 Rx/Tx 7A_0x11 20
0x12 Rx/Tx 7A_0x12 E0
0x13 Rx/Tx 7A_0x13 90
0x14 Rx/Tx 7A_0x14 00
0x15 Rx/Tx 7A_0x15 12
0x16 Rx/Tx 7A_0x16 7A
0x17 Rx/Tx 7A_0x17 36
0x18 Rx/Tx 7A_0x18 40
0x19 Rx/Tx 7A_0x19 20
0x1A Rx/Tx 7A_0x1A A0
0x1B Rx/Tx 7A_0x1B 03
0x1C Rx/Tx 7A_0x1C 90
0x1D Rx/Tx 7A_0x1D 00
0x1E Rx/Tx 7A_0x1E E9
0x1F Rx/Tx 7A_0x1F 55
0x20 Rx/Tx 7A_0x20 00
0x21 Rx/Tx 7A_0x21 00
0x22 Rx/Tx 7A_0x22 00
0x23 Rx/Tx 7A_0x23 40
0x24 Rx/Tx 7A_0x24 40
0x25 Rx/Tx 7A_0x25 00
0x26 Rx/Tx 7A_0x26 00
0x27 Rx/Tx 7A_0x27 00
0x28 Rx/Tx 7A_0x28 00
0x29 Rx/Tx 7A_0x29 00
0x2A Rx/Tx 7A_0x2A 30
0x2B Rx/Tx 7A_0x2B 0F
0x2C Rx/Tx 7A_0x2C F2
0x2D Rx/Tx 7A_0x2D 04
0x2E Rx/Tx 7A_0x2E 00
0x2F Rx/Tx 7A_0x2F 36
0x30 Rx/Tx 7A_0x30 00
0x31 Rx/Tx 7A_0x31 20
0x32 Rx/Tx 7A_0x32 11
0x33 Rx/Tx 7A_0x33 88
0x34 Rx/Tx 7A_0x34 BF
0x35 Rx/Tx 7A_0x35 1F
0x36 Rx/Tx 7A_0x36 30
0x37 Rx/Tx 7A_0x37 00
0x38 Rx/Tx 7A_0x38 00
0x39 Rx/Tx 7A_0x39 00
0x3A Rx/Tx 7A_0x3A 00
0x3B Rx/Tx 7A_0x3B 42
0x3C Rx/Tx 7A_0x3C F9
0x3D Rx/Tx 7A_0x3D 35
0x3E Rx/Tx 7A_0x3E 43
0x3F Rx/Tx 7A_0x3F C7
0x40 Rx/Tx 7A_0x40 00
0x41 Rx/Tx 7A_0x41 01
0x42 Rx/Tx 7A_0x42 04
0x43 Rx/Tx 7A_0x43 10
0x44 Rx/Tx 7A_0x44 40
0x45 Rx/Tx 7A_0x45 08
0x46 Rx/Tx 7A_0x46 02
0x47 Rx/Tx 7A_0x47 80
0x48 Rx/Tx 7A_0x48 03
0x49 Rx/Tx 7A_0x49 0C
0x4A Rx/Tx 7A_0x4A 30
0x4B Rx/Tx 7A_0x4B 41
0x4C Rx/Tx 7A_0x4C 50
0x4D Rx/Tx 7A_0x4D C0
0x4E Rx/Tx 7A_0x4E 60
0x4F Rx/Tx 7A_0x4F 90
0x50 Rx/Tx 7A_0x50 88
0x51 Rx/Tx 7A_0x51 82
0x52 Rx/Tx 7A_0x52 A0
0x53 Rx/Tx 7A_0x53 46
0x54 Rx/Tx 7A_0x54 52
0x55 Rx/Tx 7A_0x55 8C
0x56 Rx/Tx 7A_0x56 B0
0x57 Rx/Tx 7A_0x57 C8
0x58 Rx/Tx 7A_0x58 57
0x59 Rx/Tx 7A_0x59 5D
0x5A Rx/Tx 7A_0x5A 69
0x5B Rx/Tx 7A_0x5B 75
0x5C Rx/Tx 7A_0x5C D5
0x5D Rx/Tx 7A_0x5D 99
0x5E Rx/Tx 7A_0x5E 96
0x5F Rx/Tx 7A_0x5F A5
0x60 Rx/Tx 7A_0x60 00
0x61 Rx/Tx 7A_0x61 00
0x62 Rx/Tx 7A_0x62 00
0x63 Rx/Tx 7A_0x63 00
0x64 Rx/Tx 7A_0x64 00
0x65 Rx/Tx 7A_0x65 00
0x66 Rx/Tx 7A_0x66 00
0x67 Rx/Tx 7A_0x67 20
0x68 Rx/Tx 7A_0x68 00
0x69 Rx/Tx 7A_0x69 0A
0x6A Rx/Tx 7A_0x6A 22
0x6B Rx/Tx 7A_0x6B 40
0x6C Rx/Tx 7A_0x6C 00
0x6D Rx/Tx 7A_0x6D 00
0x6E Rx/Tx 7A_0x6E 00
0x6F Rx/Tx 7A_0x6F 00
0x70 Rx/Tx 7A_0x70 03
0x71 Rx/Tx 7A_0x71 20
0x72 Rx/Tx 7A_0x72 00
0x73 Rx/Tx 7A_0x73 00
0x74 Rx/Tx 7A_0x74 00
0x75 Rx/Tx 7A_0x75 00
0x76 Rx/Tx 7A_0x76 22
0x77 Rx/Tx 7A_0x77 1A
0x78 Rx/Tx 7A_0x78 00
0x79 Rx/Tx 7A_0x79 10
0x7A Rx/Tx 7A_0x7A 00
0x7B Rx/Tx 7A_0x7B 00
0x7C Rx/Tx 7A_0x7C 00
0x7D Rx/Tx 7A_0x7D 48
0x7E Rx/Tx 7A_0x7E 13
0x7F Rx/Tx 7A_0x7F 3A
0x80 Rx/Tx 7A_0x80 00
0x81 Rx/Tx 7A_0x81 E4
0x82 Rx/Tx 7A_0x82 00
0x83 Rx/Tx 7A_0x83 00
0x84 Rx/Tx 7A_0x84 00
0x85 Rx/Tx 7A_0x85 00
0x86 Rx/Tx 7A_0x86 00
0x87 Rx/Tx 7A_0x87 00
0x88 Rx/Tx 7A_0x88 00
0x89 Rx/Tx 7A_0x89 00
0x8A Rx/Tx 7A_0x8A 00
0x8B Rx/Tx 7A_0x8B 00
0x8C Rx/Tx 7A_0x8C 00
0x8D Rx/Tx 7A_0x8D 02
0x8E Rx/Tx 7A_0x8E 1C
0x8F Rx/Tx 7A_0x8F 00
0x90 Rx/Tx 7A_0x90 00
0x91 Rx/Tx 7A_0x91 00
0x92 Rx/Tx 7A_0x92 00
0x93 Rx/Tx 7A_0x93 00
0x94 Rx/Tx 7A_0x94 00
0x95 Rx/Tx 7A_0x95 00
0x96 Rx/Tx 7A_0x96 04
0x97 Rx/Tx 7A_0x97 00
0x98 Rx/Tx 7A_0x98 0C
0x99 Rx/Tx 7A_0x99 3F
0x9A Rx/Tx 7A_0x9A 3F
0x9B Rx/Tx 7A_0x9B 00
0x0 Rx/Tx 7B_0x00 00
0x1 Rx/Tx 7B_0x01 00
0x2 Rx/Tx 7B_0x02 00
0x3 Rx/Tx 7B_0x03 00
0x4 Rx/Tx 7B_0x04 01
0x5 Rx/Tx 7B_0x05 01
0x6 Rx/Tx 7B_0x06 01
0x7 Rx/Tx 7B_0x07 01
0x8 Rx/Tx 7B_0x08 60
0x9 Rx/Tx 7B_0x09 00
0xA Rx/Tx 7B_0x0A 50
0xB Rx/Tx 7B_0x0B 6F
0xC Rx/Tx 7B_0x0C 08
0xD Rx/Tx 7B_0x0D B4
0xE Rx/Tx 7B_0x0E 93
0xF Rx/Tx 7B_0x0F 69
0x10 Rx/Tx 7B_0x10 3A
0x11 Rx/Tx 7B_0x11 20
0x12 Rx/Tx 7B_0x12 E0
0x13 Rx/Tx 7B_0x13 90
0x14 Rx/Tx 7B_0x14 00
0x15 Rx/Tx 7B_0x15 12
0x16 Rx/Tx 7B_0x16 7A
0x17 Rx/Tx 7B_0x17 36
0x18 Rx/Tx 7B_0x18 40
0x19 Rx/Tx 7B_0x19 20
0x1A Rx/Tx 7B_0x1A A0
0x1B Rx/Tx 7B_0x1B 03
0x1C Rx/Tx 7B_0x1C 90
0x1D Rx/Tx 7B_0x1D 00
0x1E Rx/Tx 7B_0x1E E9
0x1F Rx/Tx 7B_0x1F 55
0x20 Rx/Tx 7B_0x20 00
0x21 Rx/Tx 7B_0x21 00
0x22 Rx/Tx 7B_0x22 00
0x23 Rx/Tx 7B_0x23 40
0x24 Rx/Tx 7B_0x24 40
0x25 Rx/Tx 7B_0x25 00
0x26 Rx/Tx 7B_0x26 00
0x27 Rx/Tx 7B_0x27 00
0x28 Rx/Tx 7B_0x28 00
0x29 Rx/Tx 7B_0x29 00
0x2A Rx/Tx 7B_0x2A 30
0x2B Rx/Tx 7B_0x2B 0F
0x2C Rx/Tx 7B_0x2C F2
0x2D Rx/Tx 7B_0x2D 04
0x2E Rx/Tx 7B_0x2E 00
0x2F Rx/Tx 7B_0x2F 36
0x30 Rx/Tx 7B_0x30 00
0x31 Rx/Tx 7B_0x31 20
0x32 Rx/Tx 7B_0x32 11
0x33 Rx/Tx 7B_0x33 88
0x34 Rx/Tx 7B_0x34 BF
0x35 Rx/Tx 7B_0x35 1F
0x36 Rx/Tx 7B_0x36 30
0x37 Rx/Tx 7B_0x37 00
0x38 Rx/Tx 7B_0x38 00
0x39 Rx/Tx 7B_0x39 00
0x3A Rx/Tx 7B_0x3A 00
0x3B Rx/Tx 7B_0x3B 43
0x3C Rx/Tx 7B_0x3C 02
0x3D Rx/Tx 7B_0x3D 35
0x3E Rx/Tx 7B_0x3E 43
0x3F Rx/Tx 7B_0x3F C7
0x40 Rx/Tx 7B_0x40 00
0x41 Rx/Tx 7B_0x41 01
0x42 Rx/Tx 7B_0x42 04
0x43 Rx/Tx 7B_0x43 10
0x44 Rx/Tx 7B_0x44 40
0x45 Rx/Tx 7B_0x45 08
0x46 Rx/Tx 7B_0x46 02
0x47 Rx/Tx 7B_0x47 80
0x48 Rx/Tx 7B_0x48 03
0x49 Rx/Tx 7B_0x49 0C
0x4A Rx/Tx 7B_0x4A 30
0x4B Rx/Tx 7B_0x4B 41
0x4C Rx/Tx 7B_0x4C 50
0x4D Rx/Tx 7B_0x4D C0
0x4E Rx/Tx 7B_0x4E 60
0x4F Rx/Tx 7B_0x4F 90
0x50 Rx/Tx 7B_0x50 88
0x51 Rx/Tx 7B_0x51 82
0x52 Rx/Tx 7B_0x52 A0
0x53 Rx/Tx 7B_0x53 46
0x54 Rx/Tx 7B_0x54 52
0x55 Rx/Tx 7B_0x55 8C
0x56 Rx/Tx 7B_0x56 B0
0x57 Rx/Tx 7B_0x57 C8
0x58 Rx/Tx 7B_0x58 57
0x59 Rx/Tx 7B_0x59 5D
0x5A Rx/Tx 7B_0x5A 69
0x5B Rx/Tx 7B_0x5B 75
0x5C Rx/Tx 7B_0x5C D5
0x5D Rx/Tx 7B_0x5D 99
0x5E Rx/Tx 7B_0x5E 96
0x5F Rx/Tx 7B_0x5F A5
0x60 Rx/Tx 7B_0x60 00
0x61 Rx/Tx 7B_0x61 00
0x62 Rx/Tx 7B_0x62 00
0x63 Rx/Tx 7B_0x63 00
0x64 Rx/Tx 7B_0x64 00
0x65 Rx/Tx 7B_0x65 00
0x66 Rx/Tx 7B_0x66 00
0x67 Rx/Tx 7B_0x67 20
0x68 Rx/Tx 7B_0x68 00
0x69 Rx/Tx 7B_0x69 0A
0x6A Rx/Tx 7B_0x6A 22
0x6B Rx/Tx 7B_0x6B 40
0x6C Rx/Tx 7B_0x6C 00
0x6D Rx/Tx 7B_0x6D 00
0x6E Rx/Tx 7B_0x6E 00
0x6F Rx/Tx 7B_0x6F 00
0x70 Rx/Tx 7B_0x70 03
0x71 Rx/Tx 7B_0x71 20
0x72 Rx/Tx 7B_0x72 00
0x73 Rx/Tx 7B_0x73 00
0x74 Rx/Tx 7B_0x74 00
0x75 Rx/Tx 7B_0x75 00
0x76 Rx/Tx 7B_0x76 22
0x77 Rx/Tx 7B_0x77 1A
0x78 Rx/Tx 7B_0x78 00
0x79 Rx/Tx 7B_0x79 10
0x7A Rx/Tx 7B_0x7A 00
0x7B Rx/Tx 7B_0x7B 00
0x7C Rx/Tx 7B_0x7C 00
0x7D Rx/Tx 7B_0x7D 48
0x7E Rx/Tx 7B_0x7E 13
0x7F Rx/Tx 7B_0x7F 3A
0x80 Rx/Tx 7B_0x80 00
0x81 Rx/Tx 7B_0x81 E4
0x82 Rx/Tx 7B_0x82 00
0x83 Rx/Tx 7B_0x83 00
0x84 Rx/Tx 7B_0x84 83
0x85 Rx/Tx 7B_0x85 00
0x86 Rx/Tx 7B_0x86 00
0x87 Rx/Tx 7B_0x87 00
0x88 Rx/Tx 7B_0x88 00
0x89 Rx/Tx 7B_0x89 02
0x8A Rx/Tx 7B_0x8A C8
0x8B Rx/Tx 7B_0x8B 00
0x8C Rx/Tx 7B_0x8C 00
0x8D Rx/Tx 7B_0x8D 02
0x8E Rx/Tx 7B_0x8E 1C
0x8F Rx/Tx 7B_0x8F 00
0x90 Rx/Tx 7B_0x90 00
0x91 Rx/Tx 7B_0x91 00
0x92 Rx/Tx 7B_0x92 00
0x93 Rx/Tx 7B_0x93 00
0x94 Rx/Tx 7B_0x94 00
0x95 Rx/Tx 7B_0x95 00
0x96 Rx/Tx 7B_0x96 04
0x97 Rx/Tx 7B_0x97 00
0x98 Rx/Tx 7B_0x98 0C
0x99 Rx/Tx 7B_0x99 3F
0x9A Rx/Tx 7B_0x9A 3F
0x9B Rx/Tx 7B_0x9B 00