Dear Sir,
In order to compensate the long cable loss, is it possible to set more bigger EQ and Diff Voltage Swing for DS90UB953?
Best regards.
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
In order to compensate the long cable loss, is it possible to set more bigger EQ and Diff Voltage Swing for DS90UB953?
Best regards.
David
Hello Tiger,
This is not possible on the SER.
However, on the DES you have the Adaptive EQ, which compensate automatecally for any loss on the transmission channel.
Please keep in mind, that you can't have more loss on the transmission channel than specified in our documentations. for example:
at 1MHz -- max 1.4dB
at 50MHz -- max 3.5dB
at 500MHz -- max 9.5dB
at 1GHz -- max 14dB
at 2GHz -- max 21.6dB