Hi, I want to know if there are any requirement on R26,R27,R28,C28 in attachment reference design?
is it ok to used resistor in 1/16W, and 50V in cap?
thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I want to know if there are any requirement on R26,R27,R28,C28 in attachment reference design?
is it ok to used resistor in 1/16W, and 50V in cap?
thank you
Hello,
Thank you for the query.
R26, R27 : 1K, 1% is recommended
R28 and C28 10% (or 5% as shown in the EVM) is recommended
Please refer to the EVM for package. Details are below
Capacitor package
Resistor package
Regards,
Sreenivasa