This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25858-Q1: Working under continuous 29V requirement?

Part Number: TPS25858-Q1

Hi Team,

Can you please check and advise with following request?

What your alternative suggestions here?

"

We have examined your TPS25858-Q1 in order to evaluate it in our automotive project, whose features I have shared in the table below.

Considering the maximum values of the product, can a 24V system work continuously under 29V input voltage?

Maximum Ratings (For One Port Only) Vin = 9-29V, Io = 3A, Vo = 5V, Pmax = 15W
Nominal Ratings (For One Port Only) Vin = 12-24V, Io = 1.5A, Vo = 5V, P = 7.5W

"

Thanks in advance

Best Regards

Furkan Sefiloglu