Hi TI Team,
Now we use TI TMDS181 in the process of plugging and unplugging HDMI cable or switching EDID black screen or flower screen situation. At present, the test shows that the communication between TMDS181 and the graphics card is OK, but the part of the signal from TMDS181 to FPGA is not good, and there is something wrong with the data received by FPGA under abnormal circumstances.
I want to ask if this problem is caused by the pull-up resistance of the AC coupling. In the TI data I saw, the resistance was all replaced by RTERM. What is the recommended resistance value?
We did not add this resistor before, so we could not run at all. Later, we found out on the forum that we should add the pull resistor, and the recommendation in the forum was 50 ohms, so now we add 50 ohms.
Is the pull-up resistor 50 ohms acceptable? Is it too big? If it is not the pull-up resistance problem, could you help to analyze it and give us some suggestions? thank you.