Hi Team,
One of our customer is using TPS65987D for their product design for power sink only + USB2.0 connection only (no Alternate Mode, no USB-3/SS link). Before adepter plug-in, TPS65987D is not power by the VIN_3V3. It is arrange to be powered from the 3.3V LDO when VBUS became available. Attached is the PD controller pjt file and the schematic for reference.
Customer hope to understand what is the expected behavior from the TPS65987D when a 5V(3A) charger (no PD negotiation) is connected. Can you help to provide your comments for below two use cases, thanks in advance.
1. a charger which advertises its current capability only via the Rp pull up resistor on the USB-C CC1 and CC2 lines.
2. a charger which does not advertise its current, just presents 5V on the Vbus line.
Thanks and regards,
Don