Other Parts Discussed in Thread: BQ25886, TPS65988
Dear Team,
I plan to use the TUSB321, BQ25886 (Battery Charger) and UBS-C connectors for the circuit with the feature below:
1. It has the intelligent wall load cube with 5V, 3A. (I.e.Apple & Samsung phones)
2. It should also be able to connect to all USB2.0, USB3.0, USB3.1 from the computer for data transfer. Is it smart enough to detect and prevent USB 2.0 over supply power because it is only provided up to 500mA.
Could you give me a sense of how these two things fit together?
Thanks in advance.
Luke Nguyen