Hi @ all,
is it possible to operate an LED with this module? My LED has a forward voltage about 6.5 V and a forward current from 10 - 30 mA. My intention is to minimize the turn-off edge of the source to some picoseconds. Ist it possible to drive such an LED with 6.5 V? In general, i will create pulses every 100 ms with an on time about 1 - 5 µs and a minimum of rising and falling edge.
Thanks in advance