Hi,
I am utilizing the TLK10034 in a design where I am using the LS side to test 16 XAUI channels. I need to produce a CRPAT and CJPAT patterns but the TLK10034 DS and app report SLLA351 give differing information. According to the DS, register 1E 0x000B, bits 11 and 5:4, Table 5-41, setting of 100 is N/A. The application report stated in Table 1 that 100 is a CRPAT short.
Which is correct?
If the DS is correct and I am supposed to use register 01 0x8002 in Table 5-100, what register do I use to check the error count for each lane?
Also, where can I find the "Test Procedures" repeatedly referred to within the DS?
Thanks,
David