Other Parts Discussed in Thread: TIC12400
Hi team.
My customer wants to apply the TIC12400-Q1 to a 36V automotive system.
To solve the input voltage range problem, the TIC12400-Q1 power supply will be supplied 12V using dc-dc.
So I want to check if there are any problems below.
1. When inputting with high signal through IN0 ~ IN9, is there any problem in function even if input by voltage distribution as shown below?
2. When 12V is spplied to VS of TIC12400-Q1, if a voltage of more then 12V(less than 35V) is input to INx, does the function of TIC12400-Q1 problem occur?
Thank you