Other Parts Discussed in Thread: TIC12400-Q1
I am trying to configure IN0 - IN10 as source pins but it is not working..... I have used the following configuration ....
using EVL software and Hardware for testing...
DEVICE_ID = 0x01000000;
INT_START = 0x02000000;
CRC = 0x0300FFFF;
IN_STAT_MISC = 0x04000000;
IN_STAT_COMP = 0x05000000;
IN_STAT_ADC0 = 0x06000000;
IN_STAT_ADC1 = 0x07000000;
IN_STAT_MATRIX0 = 0x08000000;
IN_STAT_MATRIX1 = 0x09000000;
ANA_STAT0 = 0x0A000000;
ANA_STAT1 = 0x0B000000;
ANA_STAT2 = 0x0C000000;
ANA_STAT3 = 0x0D000000;
ANA_STAT4 = 0x0E000000;
ANA_STAT5 = 0x0F000000;
ANA_STAT6 = 0x10000000;
ANA_STAT7 = 0x11000000;
ANA_STAT8 = 0x12000000;
ANA_STAT9 = 0x13000000;
ANA_STAT10 = 0x14000000;
ANA_STAT11 = 0x15000000;
ANA_STAT12 = 0x16000000;
CONFIG = 0x1A00040C;
IN_EN = 0x1BFFFFFF;
CS_SELECT = 0x1C00001F; // 0x1C0003E0;
WC_CFG0 = 0x1DB6DB6D;
WC_CFG1 = 0x1E16DB6D;
CCP_CFG0 = 0x1F000000;
CCP_CFG1 = 0x20000000;
THRES_COMP = 0x21000000;
INT_EN_COMP1 = 0x22FFFFFF;
INT_EN_COMP2 = 0x23FFFFFF;
INT_EN_CFG_0 = 0x24000004;
INT_EN_CFG_1 = 0x25000000;
INT_EN_CFG_2 = 0x26000000;
INT_EN_CFG_3 = 0x27000000;
INT_EN_CFG_4 = 0x28000000;
THRES_CFG0 = 0x29000000;
THRES_CFG1 = 0x2A016800;
THRES_CFG2 = 0x2B00D247;
THRES_CFG3 = 0x2C045C77;
THRES_CFG4 = 0x2D0CBDA2;
THRESMAP_CFG0 = 0x2E000000;
THRESMAP_CFG1 = 0x2F023000;
THRESMAP_CFG2 = 0x300001F5;
MATRIX = 0x31000000;
MODE = 0x32000000;