Hi, Team,
A customer would like to use the HD3SS6126 EVM to evaluate the DEMUX. Is there any set up to use HD3SS6126 as DEMUX?
Best Regards,
Satoshi Yone
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Team,
A customer would like to use the HD3SS6126 EVM to evaluate the DEMUX. Is there any set up to use HD3SS6126 as DEMUX?
Best Regards,
Satoshi Yone
Hello Satoshi-san,
Do you mean 2 Host and one device?. I am not aware of that however, the customer can use adapters or custom cables to achieve the connectivity (please use short cables, considering that both options may impact the signal integrity).
Regards,
Diego.
Hi Diego-san,
Sorry for interrupt you, but I would like you to confirm about your answer.
* According to schematic of EVM, PMOS FET exist b/w U20 and U2,U21. So, following behavior will happen to realize MUX/DEMUX finction on this EVM.
1. When USB host is Micro-B side(U2, U21), Vbus comes from U2 or U21 (Or both), and PMOS will be switched on by this voltage(Source -> Drain).
2. Conversely, when USB host is Micro-A side(U20), Vbus comes from U20, and I guess that PMOS of Drain-Source will conduct through parasitic diode of PMOS. In this case, i think that voltage drop will happen on VBUS line (in general, Vf = 0.6 or 0.7V).
Then, I have following question.
* In case of above "2", If 5V(Vbus typ) is supplied to EVM, dropped Vbus voltage may drop below min voltage(4.4V).
So, should user care this voltage drop by user itself ?
Thanks in advance,
Machida
Hello Machida-san,
For testing purposes, I think that the best option is to remove the power switches and short the VBUS path. It is not the best case for a final product, however, in a controlled environment, you can have the VBUS path clear.
Regards,
Diego.