Hi Team
I find TUSB1002 host to redriver length/redriver to conn length are 8/2 inch,is it the max length requirement? [ spec 8.2.1 ]
our system current topology is 12.4/1 inch with 2 via. Can TUSB1002 support this topology.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team
I find TUSB1002 host to redriver length/redriver to conn length are 8/2 inch,is it the max length requirement? [ spec 8.2.1 ]
our system current topology is 12.4/1 inch with 2 via. Can TUSB1002 support this topology.
Hi Kerr,
The TUSB1002 is capable to compensate up to 15dB of loss and has an output swing of 1.2V. The spec 8.2.1 is only a reference example design. Could you provide the insertion parameter of your traces?
Best Regards,
Luis Omar Moran
High Speed Interface
SWAT Team