Part Number: TPS65983EVM
Hi,
We made our board which has TPS65981 PD controller. After bring-up, I have flashed 5V/2A sink application image into the TPS65981 SPI boot memory. To test its compatibility with PD sourcing device, I have tried working TPS65983 EVM as a power source detailed below for your understanding.
1. Flashed a TI reference Downstream Facing Port image with 5V/2A source PDO in EVM.
2. 3.3V power supply is given to VIN_3V3 for TPS65983 operation. A 5V/2A power is provided on PPHV path.
3. TI EVM and our board are connected through Type-C to Type-C cable.
The expected behavior is TI TPS65983 EVM should establish a PD contract with our board and source 5V/2A (from PPHV). However, our boards remain unpowered. We observe that PPHV does not pass through the VBUS on TI EVM itself. I'm not certain whether I'm missing any software configurations or proper hardware setup.
Could you please assist us in configuring the TPS65983 EVM as PD sourcing device in detail?
Regards,
Manikandan