Hi, we are using the TPS65982 for our PD charger application (sink power delivery from type C port). On initial power up with 20V external plugged in from the type C port, the battery charges as expected, when the external power is removed, the battery power kicks in to supply system power, however, once the external power is plugged back in a few seconds later, the PD controller is unable to renegotiate. We are assuming the negotiation is done automatically. As a side note, the VDDIO and VIN_3V3 are connected to an on-board 3.3V supply instead of using the controller's LDO_3V3. Would this impact the behavior we are seeing?
We'll try to repeat this using the EVM board, but in the meantime, would connecting VDDIO and VIn3v3 this way cause the issue we are seeing?
Thanks.