Other Parts Discussed in Thread: TUSB4041I
Hello,
I was looking into the TUSB2077A 7-port Hub for universal Serial Bus (TUSB2077A 7-Port Hub for the Universal Serial Bus With Optional Serial EEPROM Interface. but it looks like a very old part would you recommend a new solution for my following requirements:
Prompt: USB hub port for testing equipment able to handle constant use for long periods of time.
- IC (and all other parts) are large enough to hand replace. (no gnd pad under the IC)
- >=7 ports
- 2.0 USB
- Can supply from Vbus line a >= 200mA draw
- ESD protection and over voltage protection on all lines (I have had a lot of issue with this part in the past)
- Dev kit to test on, layout reference and parts reference (preferred)
Generally the more ports the better.
Regards,
David