Hi,
If in the case of unused below pin, which these pin correct for Open or Pulldown?
・Pin2 DM_HOST
・Pin3 DP_HOST
・Pin4 CHG_AL_N
・Pin10 CHG_DET
Best Regards,
Yusuke/Japan Disty
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
If in the case of unused below pin, which these pin correct for Open or Pulldown?
・Pin2 DM_HOST
・Pin3 DP_HOST
・Pin4 CHG_AL_N
・Pin10 CHG_DET
Best Regards,
Yusuke/Japan Disty
The CHA_AL_N is required to have a 10K pull up. The CHG_DET should have a 10K pull down. In what application are you using the BQ24392 without DP_HOST and DM_HOST connected?
Michael-san,
Thank you for your response and support.
Application is battery charger.
Customer wants to detect CDP/SDP using bq24392.
Other detection and control are performed by MUC.
If in the case of unused below pin, which these pin correct for Open or Pulldown?
・Pin2 DM_HOST
・Pin3 DP_HOST
Best Regards,
Yusuke/Japan Disty
Michael-san,
Thank you for your kind support.
Let me ask you one more thing.
"The CHG_AL_N is required to have a 10K pull up.
The CHG_DET should have a 10K pull down."
However,
・Pin4 CHG_AL_N is open drain.
・CHG_DET is push-pull.
Please tell me the disadvantage of setting these two terminals to OPEN.
Customers want to OPEN processing in order to reduce the cost and board area.
Could you give me your advice?
Best Regards,
Yusuke/Japan Disty
Hi,
Can I get the information?
Customers need that information for design.
If you need more information or if I should clarify my comment ,
please let me know.
Best Regards,
Yusuke/Japan Disty
Michael-san,
Thank you for you kind support.
I am sorry I didn't explain it clearly enough.
Customer wants bq24392 to detect only DCP or SDP/CDP
Customer use bq24392 with 5 pins and 1 pin pulled up.
DCP is high, and SDP / CDP high and low are distinguished.
The customer made a detection by this.
----------------
・Pin4 CHG_AL_N is open drain.
・CHG_DET is push-pull.
Please tell me the disadvantage of setting these two terminals to OPEN.
----------------
Could you give me your advice?
Best Regards,
Yusuke/Japan Disty