Hellow! We have some problems with SN74LVC2T45MDCTTEP (DUAL-BIT DUAL-SUPPLY BUS TRANSCEIVER WITH CONFIGURABLE VOLTAGE TRANSLATION AND 3-STATE OUTPUTS) with marking NXR59Z on the top of device, and much more less problems with the same device, but with marking NXR72Z.
So, there is question: what does this marking means?
there are not much information about it in datashit :
"(4) There may be additional marking, which relates to the logo, the lot trace code information, or the environmental category on the device.
(5) Multiple Device Markings will be inside parentheses. Only one Device Marking contained in parentheses and separated by a "~" will appear on a device. If a line is indented then it is a continuation of the previous line and the two combined represent the entire Device Marking for that device."