Other Parts Discussed in Thread: SN65HVD1792
Hello
I am designing RS-422 interface circuit using ISO1432.
(3.3V power is supplied to the VCC2 pin on ISO1432)
5V power is supplied to the RS-422 transceiver IC, which is the component of the communication partner.
The supply voltage is different from the component of the communication partner, but let me check that there is no problem.
(It is within the range of VID (-15V to +15V) and VI (-7V to +12V) described in the ISO1432 data sheet and I think that there is no problem, but please check it just in case)
Regards,
MESH