This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1450: ISO1450 transmit distance questions

Part Number: ISO1450

Hi experts,

My customer now use our ISO1450, and they have some questions about transmit distance, and since I don't know enough about ISO1450, so I need your help to answer our customer this time.

1. What is the maximum communication distance ISO1450 can transmit?
2. How many devices can be mounted on ISO1450 at most
3. Is the matching resistance(between A and B pin) of ISO1450 related to the communication distance, or how does the matching resistance match the distance?

Because customer needs are more urgent, please reply to me as soon as possible, thanks.

Best regards,

Andy Liu