hi sir
I need a relay signal detect with isolation
survey the TI/ ISO1212, & Max22518
The max22518 Power consumption Is less than TI ,Right
The ISO1212 output is postive logic output, when input is high, right?
if the input is high, i hope the output is negative logic output, may i do the setup?
thanks