Other Parts Discussed in Thread: SN65HVD230,
Hi Team,
I saw ISO1050 and SN65HVD230`s output voltage level is different as below:
ISO1050
SN65HVD230
So I am wonder can ISO1050 communicate with SN65HVD230?
Thanks.
Regards, Sunny
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I saw ISO1050 and SN65HVD230`s output voltage level is different as below:
ISO1050
SN65HVD230
So I am wonder can ISO1050 communicate with SN65HVD230?
Thanks.
Regards, Sunny
Hi Sunny,
Thank you for reaching out.
CAN is a differential interface and the voltage difference needs to meet the CAN Dominant and Recessive state thresholds and both these devices meet those thresholds and the absolute voltage on the bus doesn't impact CAN communication. Even a 3.3V CAN device can be connected to 5V CAN device without any issues. Thanks.
Regards,
Koteshwar Rao