Hi,
Could you please let me know about ICC2 consumption. Datasheet show as below:
- TXD = 0 V, bus dominant, RL = 60 Ω: 73.4 mA(MAX)
- TXD= VCC1, bus recessive, RL = 60 Ω: 4.1 mA(MAX)
In common use case, some nodes connect to CAN Bus line and one of then is active. I guess the node which is Active consume 73.4mA as Maximum. But how much current other nodes which aren't active consume? Should user consider the consumption as 4.1mA? or should he consider it as 73.4mA even if the nodes aren't active?
I would like to select power supply requirement for ICC2.
Regards,
Nagata.