Due to the U.S. Thanksgiving holiday, please expect delayed responses during the week of 11/22.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7842: Differen ISO7842 to ISO7742

Part Number: ISO7842
Other Parts Discussed in Thread: ISO7742

Hi,

what is the difference between ISO7842 and ISO7742?

thanks

fred

  • Hi Fred:

    Thanks for posting your question on E2E!

    ISO7742 is our latest generation, 100Mbps and most robust EMC digital isolator. The key difference between ISO7842 and ISO7742 is that ISO78xx family of devices are rated for 5.7kVrms while ISO77xx family is 5kVrms. The rest of the electrical and HV specs are similar.

    I'd recommend ISO7742 for newer designs as long as 5kVrms is adequate for your application.

    Regards,

    Dushmantha